cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure Timer input XOR for STM32G030K6T6 Microcontroller ?

Sudhakar.R
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3


_legacyfs_online_stmicro_images_0693W00000bkHuLQAU.pngJW

Sudhakar.R
Associate III

Thank you for your response.

I tried with the STM32F1 series it worked well. when I did with the STM32G030K6t6 it doesn't work

when there is any change in the input TIM counter(xor timer) reset to zero but it doesn't work in STM32G030K6t6

below I have attached my initialization TIM3 for the XOR operation

void MX_TIM3_Init(void)
{
 
  /* USER CODE BEGIN TIM3_Init 0 */
 
  /* USER CODE END TIM3_Init 0 */
 
  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_HallSensor_InitTypeDef sConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};
 
  /* USER CODE BEGIN TIM3_Init 1 */
 
  /* USER CODE END TIM3_Init 1 */
  htim3.Instance = TIM3;
  htim3.Init.Prescaler = 65535;
  htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim3.Init.Period = 65535;
  htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
  sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
  sConfig.IC1Filter = 0;
  sConfig.Commutation_Delay = 0;
  if (HAL_TIMEx_HallSensor_Init(&htim3, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC2REF;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM3_Init 2 */
 
  /* USER CODE END TIM3_Init 2 */
 
}

Read out and check/compare-to-working/post content of TIM registers.

JW