cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure GPDMA in STM32H563ZI for USART

Shubham08
Associate III

I am using Nucleo-H563ZI in this. I was configuring USART6 in DMA mode, but for this controller instead of DMA, there was GPDMA1/2. Currently, I have configured it in GPDMA1. The module is EC200. I am transmitting AT but am not getting the response that it is OK. Therefore, I am not sure whether the USART is correctly configured or not

Shubham08_0-1742092615394.png

Shubham08_1-1742092687622.png

Shubham08_2-1742092740710.png

Shubham08_3-1742092793406.png

Shubham08_4-1742092809933.png

/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define EC200_RX_SIZE 16
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

COM_InitTypeDef BspCOMInit;

UART_HandleTypeDef huart4;
UART_HandleTypeDef huart6;
DMA_HandleTypeDef handle_GPDMA1_Channel1;
DMA_HandleTypeDef handle_GPDMA1_Channel0;

/* USER CODE BEGIN PV */
uint8_t EC200_TX[] = "AT\r\n";
uint8_t EC200_RX[16] = {0};

volatile uint8_t TxComplete = 0; // Separate flag for TX
volatile uint8_t RxComplete = 0; // Flag for RX

int isSent = 1;
int countloop =0;
int countinterrupt = 0;
//uint8_t RxComplete = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_UART4_Init(void);
static void MX_ICACHE_Init(void);
static void MX_USART6_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
//void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
//{
////	isSent = 1;
//	countinterrupt++;
//	HAL_UART_Receive_DMA(&huart6, EC200_RX, 4);
//}
//
//void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
//{
//    // Set flag to indicate reception complete
//    RxComplete = 1;
//    // Ready to send next command
//    isSent = 1;
//}

// 3. In your TX callback, use the consistent buffer size:
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
    if(huart == &huart6)
    {
        TxComplete = 1;
        countinterrupt++;

        // Start receiving with consistent buffer size
        HAL_UART_Receive_DMA(&huart6, EC200_RX, EC200_RX_SIZE);
    }
}

// 4. Add debug output in your RX callback
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
    if(huart == &huart6)
    {
        RxComplete = 1;


        // Toggle LED for visual confirmation
        BSP_LED_Toggle(LED_YELLOW);

        // Set flag to send next command after a delay
        isSent = 1;
    }
}

// Add error callback to catch DMA errors
void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
{
    if(huart == &huart6)
    {
        // Toggle RED LED rapidly to indicate error
        for(int i=0; i<10; i++) {
            BSP_LED_Toggle(LED_RED);
            HAL_Delay(100);
        }

        // Reset flags
        isSent = 1;
    }
}
/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_GPDMA1_Init();
  MX_UART4_Init();
  MX_ICACHE_Init();
  MX_USART6_UART_Init();
  /* USER CODE BEGIN 2 */
  HAL_UART_Receive_DMA(&huart6, EC200_RX, 10);
  /* USER CODE END 2 */

  /* Initialize leds */
  BSP_LED_Init(LED_GREEN);
  BSP_LED_Init(LED_YELLOW);
  BSP_LED_Init(LED_RED);

  /* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
  BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);

  /* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
  BspCOMInit.BaudRate   = 115200;
  BspCOMInit.WordLength = COM_WORDLENGTH_8B;
  BspCOMInit.StopBits   = COM_STOPBITS_1;
  BspCOMInit.Parity     = COM_PARITY_NONE;
  BspCOMInit.HwFlowCtl  = COM_HWCONTROL_NONE;
  if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
  {
    Error_Handler();
  }

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
//	 if(isSent == 1)
//	 {
//		 HAL_UART_Transmit_DMA(&huart6, EC200_TX, strlen((char*)EC200_TX));
//		 isSent = 0;
//	 }

	  if(isSent == 1)
	      {
		  	  TxComplete = 0;
			  RxComplete = 0;

			  memset(EC200_RX, 0, sizeof(EC200_RX));


	          // Send AT command
	          if (HAL_UART_Transmit_DMA(&huart6, EC200_TX, strlen((char*)EC200_TX)) == HAL_OK)
	          {
	              isSent = 0;
	          }
	          else
	                  {
	                      // If DMA transmission fails, show error
	                      for(int i=0; i<5; i++) {
	                          BSP_LED_Toggle(LED_YELLOW);
	                          HAL_Delay(200);
	                      }
	                  }
	      }

//	      if(RxComplete == 1)
//	      {
//	          // Process received data - should be "OK\r\n"
//	          // Ensure null termination for string functions
//	          EC200_RX[4] = '\0';
//
//	          // Forward to debug port
////	          BSP_COM_Write(COM1, EC200_RX, 4);
//
//	          // Reset flag after processing
//	          RxComplete = 0;
//	      }

	 BSP_LED_Toggle(LED_RED);
	 HAL_Delay(500);
	 countloop++;

  }
}

 

 

 

2 REPLIES 2
psabela
Associate II

Try to enable FIFO mode on USART.   

Guenael Cadier
ST Employee

Hi @Shubham08 

You could also try to declare isSent variable as volatile (as used in both main and interrupt routines). Depending on your code optimizations options, it could help.
Another comment : in your code your mentioned COM_WORDLENGTH_8B : 8B is nb of data + parity, so as no parity check is enabled, it means 8B data, not 7 (nb of stop bits is not part of Wordlength.
regards