2023-05-08 11:17 PM - last edited on 2024-07-05 04:58 AM by SofLit
Both CAN buses are transmitting correctly. But when I initialize CAN1 and CAN2 only CAN2 receives messages, when only CAN2 is initialized it receives. same for the CAN1. Here I attached my initializing function.
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 16;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_5TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
CAN_FilterTypeDef can_filter_config1;
can_filter_config1.FilterActivation = CAN_FILTER_ENABLE;
can_filter_config1.FilterBank = 10;
can_filter_config1.FilterFIFOAssignment = CAN_FILTER_FIFO0;
can_filter_config1.FilterIdHigh = 0;
can_filter_config1.FilterIdLow = 0x0000;
can_filter_config1.FilterMaskIdHigh = 0;
can_filter_config1.FilterMaskIdLow = 0x0000;
can_filter_config1.FilterMode = CAN_FILTERMODE_IDMASK;
can_filter_config1.FilterScale = CAN_FILTERSCALE_32BIT;
can_filter_config1.SlaveStartFilterBank = 0;
HAL_CAN_ConfigFilter(&hcan1, &can_filter_config1);
/* USER CODE END CAN1_Init 2 */
}
/**
* @brief CAN2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_CAN2_Init(void)
{
/* USER CODE BEGIN CAN2_Init 0 */
/* USER CODE END CAN2_Init 0 */
/* USER CODE BEGIN CAN2_Init 1 */
/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 16;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_5TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = DISABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = DISABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
CAN_FilterTypeDef can_filter_config2;
can_filter_config2.FilterActivation = CAN_FILTER_ENABLE;
can_filter_config2.FilterBank = 1;
can_filter_config2.FilterFIFOAssignment = CAN_FILTER_FIFO1;
can_filter_config2.FilterIdHigh = 0;
can_filter_config2.FilterIdLow = 0x0000;
can_filter_config2.FilterMaskIdHigh = 0;
can_filter_config2.FilterMaskIdLow = 0x0000;
can_filter_config2.FilterMode = CAN_FILTERMODE_IDMASK;
can_filter_config2.FilterScale = CAN_FILTERSCALE_32BIT;
can_filter_config2.SlaveStartFilterBank = 1;
HAL_CAN_ConfigFilter(&hcan2, &can_filter_config2);
/* USER CODE END CAN2_Init 2 */
}
Solved! Go to Solution.
2023-05-24 02:33 AM
Hello,
You have an issue with filter config:
.SlaveStartFilterBank parameter you have to configure it once and it determines the filter allocation for both CAN1 and CAN2. Assimilate it as a cursor.
.FilterBank should be configured according to .SlaveStartFilterBank.
I'm attaching a text file that explains the principal.
Hope it helps
2023-05-24 02:14 AM
Hello @SPeri.1 ,
which board do you use ?
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-24 02:20 AM
Hello @SPeri.1 ,
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-24 02:33 AM
Hello,
You have an issue with filter config:
.SlaveStartFilterBank parameter you have to configure it once and it determines the filter allocation for both CAN1 and CAN2. Assimilate it as a cursor.
.FilterBank should be configured according to .SlaveStartFilterBank.
I'm attaching a text file that explains the principal.
Hope it helps
2023-05-29 08:40 PM
STM32F105RCT6
2023-05-29 08:59 PM
Now i get it. Thank you so much.