cancel
Showing results for 
Search instead for 
Did you mean: 

Transmit message ids on stm32f407 board in CAN Communication

rohitkumarkv07
Associate III

I have tried to transmit message through stm32f407 and want to see the signals. But I am not able to see that in logic analyzer. Can you help me out.

#include "Mcu.h"
#include "stm32f4xx.h"
#include "Mcu_RegTypes.h"
#include "Mcu_InternalTypes.h"

void CAN1_Init(void);
void CAN1_Tx(uint8_t tr);
uint8_t CAN1_Rx(void);
void TIM4_ms_Delay(uint32_t delay);
uint8_t k = 0;
uint8_t rec = 0;


void GPIO_Init(){
	// Enable GPIOB clock signal
	//RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN;

	// Configuring PD0 and PD1 in alternate function mode
	GPIOD->MODER |= GPIO_MODER_MODE1_1  | GPIO_MODER_MODE0_1 ;

	// Selecting AF9 for PD0 and PD1 (See Page 272 of dm00031020)
	GPIOD->AFR[1] |= (GPIO_AFRL_AFSEL0_3 | GPIO_AFRL_AFSEL0_1 | GPIO_AFRL_AFSEL1_0 | GPIO_AFRL_AFSEL1_3);
}

void CAN1_Init(){
	/* 1. Setting Up the Baud Rate and Configuring CAN1 in*/

	// Enable clock for CAN1
	RCC->APB1ENR |= RCC_APB1ENR_CAN1EN;

	// Entering CAN Initialization Mode and wait for acknowledgment
	CAN1->MCR |= CAN_MCR_INRQ;
	while (!(CAN1->MSR & CAN_MSR_INAK)){}

	//Set Loop back mode for CAN1
	CAN1->BTR &= ~CAN_BTR_LBKM;

	//Setting the Re synchronization jump width to 1
	CAN1->BTR &= ~CAN_BTR_SJW;

	//Setting the no. of time quanta for Time segment 2
	// TS2 = 4-1;
	CAN1->BTR &= ~(CAN_BTR_TS2);
	CAN1->BTR |= (CAN_BTR_TS2_1 | CAN_BTR_TS2_0);

	//Setting the no. of time quanta for Time segment 1
	// TS1 = 3-1;
	CAN1->BTR &= ~(CAN_BTR_TS1);
	CAN1->BTR |= (CAN_BTR_TS1_1);

	//Setting the Baud rate Pre-scalar for CAN1
	// BRP[9:0] = 16-1
	CAN1->BTR |= ((16-1)<<0);

	// Exit the Initialization mode for CAN1
	// Wait until the INAK bit is cleared by hardware
	CAN1->MCR &= ~CAN_MCR_INRQ;
	while (CAN1->MSR & CAN_MSR_INAK){}

	//Exit Sleep Mode
	CAN1->MCR &= ~ CAN_MCR_SLEEP;
	//while (CAN1->MSR & CAN_MSR_SLAK);

	/* 2. Setting up the Transmission----------------------------------------*/

	CAN1->sTxMailBox[0].TIR = 0;

	//Setting up the Std. ID

	CAN1->sTxMailBox[0].TIR = (0x01 << 21);


	CAN1->sTxMailBox[0].TDHR = 0;

	// Setting Data Length to 1 Byte.
	CAN1->sTxMailBox[0].TDTR = 1;

	/* 3. Configuring the Filters--------------------------------------------*/

	//Enter Filter Initialization mode to configure the filters
	CAN1->FMR |= CAN_FMR_FINIT;

	// Configuring the Number of Filters Reserved for CAN1
	// and also the start bank for CAN2
	CAN1->FMR |= 14<<8;


	// Select the single 32-bit scale configuration
	CAN1->FS1R |= CAN_FS1R_FSC13;

	// Set the receive ID
	//CAN1->sFilterRegister[13].FR1 = 0x0; // Accept any message ID
	CAN1->sFilterRegister[0].FR1 = (0x01 << 21);

	// Select Identifier List mode
	CAN1->FM1R &= ~CAN_FM1R_FBM13; // Use mask mode

	//Activating filter 13
	//CAN1->FA1R |= CAN_FA1R_FACT13;
	CAN1->FA1R |= (1 << 0) | (1 << 1) | (1 << 2) | (1 << 3);

	//Exit filter Initialization Mode
	CAN1->FMR &= ~CAN_FMR_FINIT;
}

void CAN1_Tx(uint8_t tr){
	// Put the Data to be transmitted into Mailbox Data Low Register
	CAN1->sTxMailBox[0].TDLR = tr;

	// Request for Transmission
	CAN1->sTxMailBox[0].TIR |= 1;

}

uint8_t CAN1_Rx(){
	// Monitoring FIFO 0 message pending bits FMP0[1:0]
	//while(!(CAN1->RF0R & 3)){}

	// Read the message ID from the FIFO 0 mailbox
	uint32_t RIR = CAN1->sFIFOMailBox[0].RIR;
	uint8_t RxD = (CAN1->sFIFOMailBox[0].RDLR) & 0xFF;

	// Extract message ID from RIR
	uint32_t msgID = RIR >> 21;

	// Releasing FIFO 0 output mailbox
	CAN1->RF0R |= 1 << 5;

	return msgID;
}


int main()
{
	
	Mcu_Init(&Mcu_ConfigSet[0]);
	Mcu_InitClock(0);
	while (MCU_PLL_LOCKED != Mcu_GetPllStatus());
	Mcu_DistributePllClock();
	GPIO_Init();
	CAN1_Init();




	while (1)
	{

		// Main program loop
		CAN1_Tx(k);
		rec = CAN1_Rx();
		k += 1;
		if (k > 25)
			k = 0;
	}
}
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

You need to configure GPIOs even in loopback mode + Rx pin set at pull-up but you disabled the RCC clock for GPIOB!

PS: again: please start with a HAL example to at least validate the HW and inspire from it for your register level programming.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

You need to configure GPIOs even in loopback mode + Rx pin set at pull-up but you disabled the RCC clock for GPIOB!

PS: again: please start with a HAL example to at least validate the HW and inspire from it for your register level programming.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.