2021-05-21 11:13 PM
Board : STM32F469I
I created a project via cubemx. how to use QSPI memory for structure variables. I am struggled for this issue.
Thanks
D. Manikandan
Solved! Go to Solution.
2021-06-09 4:13 AM
Hello @Mani ,
What is the type of QSPI memory ?
Please precise what do you expect exactly as result?
As I understood your need to change variable in the external QSPI memory.
So, you can follow and get inspired from QSPI_perfs example within X-CUBE-PERF-H7, it is based on STM32H7 , but you can update it according to your needs.
But for your information: QSPI cannot support memory mapped write.
The Memory-mapped mode is used in below cases:
• For reading operations
• For code execution from external Quad-SPI Flash memory
You can also refer to this AN4760 Application note Quad-SPI interface on STM32 microcontrollers and microprocessors.
Imen
2021-06-09 4:13 AM
Hello @Mani ,
What is the type of QSPI memory ?
Please precise what do you expect exactly as result?
As I understood your need to change variable in the external QSPI memory.
So, you can follow and get inspired from QSPI_perfs example within X-CUBE-PERF-H7, it is based on STM32H7 , but you can update it according to your needs.
But for your information: QSPI cannot support memory mapped write.
The Memory-mapped mode is used in below cases:
• For reading operations
• For code execution from external Quad-SPI Flash memory
You can also refer to this AN4760 Application note Quad-SPI interface on STM32 microcontrollers and microprocessors.
Imen
2021-06-16 11:25 PM
This is very helpful for me. Thanks