2019-03-14 5:28 PM
I have a LSE with a freq of 32.768KHz. The cube generated code uses values for
AsynchPrediv = 127;
SynchPrediv = 255;
These values give around ~4ms resolution. Is it possible to get to ~1ms resolution?
Thanks
2019-03-14 6:57 PM
Do you intend to use RTC only for msec delay? Otherwise a low power timer based on HSE should do the job.
2019-03-14 7:08 PM
I'm using the RTC to get a time stamp down to the millisecond for data logging purposes. Is there a way to synchronize a low power timer with the RTC?
Thanks!
2019-03-15 3:31 AM
Change the ratio between asynchronous and synchronous prescaler. Cut asynchronous down to a quarter of what's now (don't forget that the value in register is one less than the dividing ratio) and compensate by increasing the synchronous by the same factor.
JW