cancel
Showing results for 
Search instead for 
Did you mean: 

How many 32 bit timers does STM32H573 have? 2 or 4? Conflicting information in data sheet

F71334
Associate II

Hello,

I'm refering to DS14121 Rev 1 of STM32H573xx. 

- "Figure 1. STM32H573xx block diagram" shows 4 32 bit timers (TIM2, TIM3, TIM4, TIM5)

- "Table 2. STM32H573xx features and peripheral counts" says there are only two.

Where can I find trustworthy information on the correct number?

Have a nice day,

F

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

From RM0481:

SofLit_0-1702541763166.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

10 REPLIES 10
SofLit
ST Employee

Hello,

From RM0481:

SofLit_0-1702541763166.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

btw

Fig.1 , block diagram  has a lot of extra memory :)

 

AScha3_0-1702542325033.png

512 KB !  or 512 byte, as in text... ?? maybe STM should look here too.

If you feel a post has answered your question, please click "Accept as Solution".

Yes indeed it's a typo and it will be fixed in coming revisions of the DS. Thank you for raising this up :).

Internal ticket number for tracking: 168793

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
F71334
Associate II

What does "typically" mean? Is there any STM32H573 that has four 32 bit timers?

AScha.3
Chief III

where are the missing 2 x 32 bit counters?

tim2 + 5 are 32 bit:

AScha3_0-1702553032942.png

tim 3 + 4 are 16 bit:

AScha3_1-1702553272611.png

 

 

and where the other 32 bit counters ?

If you feel a post has answered your question, please click "Accept as Solution".

@F71334 ,

"Yes indeed it's a typo and it will be fixed in coming revisions of the DS. Thank you for raising this up :)"

Was an answer to @AScha.3  regarding the FMAC RAM size. And there is no issue in our documentations regarding Timers. As shown in the reference manual in "TIM2/TIM3/TIM4/TIM5 introduction" section, it was said "16-bit or 32-bit". So there are two 16-bit timers and two 32-bit timers as shown in Table 397.

The best answer for your request is the first one I've already provided.

Thank you.

 

.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

I'm talking about this:

tim.png

As mentioned, "Figure 1. STM32H573xx block diagram".

Sorry for any inconvenience.

 

 

SofLit
ST Employee

OK. Now it's clear. It  will be fixed in coming revisions of the DS. It will be treated in the same ticket number: 168793.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

It is literally the first issue reported in the second sentence of the head post. But, of course, who could notice such a "hidden" text...