2023-12-14 12:00 AM
Hello,
I'm refering to DS14121 Rev 1 of STM32H573xx.
- "Figure 1. STM32H573xx block diagram" shows 4 32 bit timers (TIM2, TIM3, TIM4, TIM5)
- "Table 2. STM32H573xx features and peripheral counts" says there are only two.
Where can I find trustworthy information on the correct number?
Have a nice day,
F
Solved! Go to Solution.
2024-09-26 02:29 AM
@AScha.3 wrote:
btw
Fig.1 , block diagram has a lot of extra memory :)
512 KB ! or 512 byte, as in text... ?? maybe STM should look here too.
Hello @AScha.3 ,
This typo is fixed in the DS14121 rev 3.
Thank you.