2021-02-19 11:34 AM
I used an LSE component proven out on another design containing a STM32F412 for a new design using a STM32L433. The LSE part is Abracon ABS06-32.768kHz-6 which is listed in AN2867 as compatible with the L4 family. I'm using the HAL_RCCEx_EnableLSCO() function to pipe out my LSE signal and it is underwhelming. The duty cycle is roughly 40/60 and while the period is close, it's not as consistence as I would expect. I have tried changing the drive strength with the __HAL_RCC_LSEDRIVE_CONFIG() function. While the raw signal at the crystal looks better, the piped output doesn't improve when adjusting the drive strength. Drive strength is the only difference I can think of between the STM32F412 design and mine as the low drive for it is 1uA and the high drive for the STM32L433 is 630nA. Is there something else I am missing in software or in my crystal selection to explain the difference in performance?
The layout is tight and I also have CSS turned off per the errata notes.
Thanks,
Lauren
2021-02-19 12:39 PM
What load capacitors are you using?
ST's NUCLEO uses an NDK NK3215SA 32.768 Khz 6pF, with a pair of 6.8pF
That's probably on the high side, depending on what the stray capacitance looks like.
I'd probably try a couple of different values in your board/circuit as built and see if you can improve things that way.
2021-03-01 9:37 AM
Hi @LAdam.1
I confirm the ABS06-32.768kHz-6 is compatible with STM32L4.
In deed, you can refer to AN2867, section "3.4 Oscillator transconductance" to calculate gmcrit. Then, check if Gm_crit_max > gmcrit. The Gm_crit_max is provided in STM32L4 datasheet, Table 57 "LSE oscillator characteristics (fLSE = 32.768 kHz)".
Also, you can refer to section "3.3 Load capacitance" to calculate the external capacitors.
What drive mode did you use?
Bouraoui
2021-03-02 8:10 AM
I have tied every mode level, and they all gave about the same response. technically driving at anything about LOW will meet the gmcrit criteria. When I measure the piped out value of my LSE signal my average frequency is close to expected, but the range of frequencies is very wide at around 32.3kHz-33.3kHz.
2021-03-03 12:09 AM
To make sure that Gm_crit_max > gmcrit, I suggest to use Medium low drive mode.
What is the value of the used external capacitors (CL1 and CL2)?
Bouraoui
2021-03-03 6:38 AM
My CLs are 6.8pF. I tried lowering them without a noticeable difference in my output signal.
2021-03-03 2:15 PM
Tell us more about your hardware. What is the power supply? Are there any power components around? Or any high-frequency circuitry? Can you post the layout of the crystals surroundings?
JW