cancel
Showing results for 
Search instead for 
Did you mean: 

How can it be that the amount of lines of code in main() affect the time it takes to execute an interrupt routine?

MB7
Associate II

Hi community,

This question is all about the behavior of the DMA1_Channel1_IRQHandler in my application.

I am working with an STM32G431CBT. It is running at 168MHz. Configured with 4 Flash wait states.

NVIC interrupt priorities are setup using CMSIS functions as follows:

SystemCoreClockUpdate();
clock = SystemCoreClock;
SysTick_Config(clock/1e3);
 
NVIC_SetPriorityGrouping(0);
 
NVIC_DisableIRQ(SysTick_IRQn);
irq_prio = NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 10, 0);
NVIC_SetPriority(SysTick_IRQn, irq_prio);
NVIC_EnableIRQ(SysTick_IRQn);
 
irq_prio = NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 13, 0);
NVIC_SetPriority(USART2_IRQn, irq_prio);
NVIC_EnableIRQ(USART2_IRQn);
 
irq_prio = NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0); //highest priority!!!
NVIC_SetPriority(DMA1_Channel1_IRQn, irq_prio);
NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 
 

TIM1->CCR5 (on match) triggers ADC conversion sequence. ADC triggers DMA1_Channel1 (circular, periph-to-mem). DMA1 is setup to issue an interrupt on transfer complete (TCIE).

The DMA1_Channel1_IRQHandler (has highest priority) then fires and a few things are processed and calculated within it.

My code compiles with no errors and warnings. And as far as I can see it all works as intended.

But here comes the strange thing:

Right at the start of DMA1_Channel1_IRQHandler I set a GPIO Pin high. At the End of DMA1_Channel1_IRQHandler I set the same Pin low. Looking at the generated high-low pulse with an oscilloscope I can measure the execution time of the DMA1_Channel1_IRQHandler. It takes 1.69µs.

But if I shrink the code in the main() by a few lines of code I can see that the execution time gets lower!!! :o And if I put just an empty while(1) loop in the main() execution time gets even lower....to its lowest-->1.22µs !!!!:o

How can that be? An ISR should not be affected in such a way by the amount of code in a low priority function just like main().

Anybody any ideas on that?

Cheers

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Check alignment of IRQHandlers, and related call-back functions.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal

Put the interrupts in a different C file than main, otherwise the compiler just optimized too much by not needing to save/restore core registers on stack.

gregstm
Senior III

Try creating an interrupt handler that does the bare minimum besides setting the GPIO bits, that is no calls, write straight to the registers. Perhaps something is branching within the interrupt handler (perhaps within a routine the interrupt handler calls). You say the timing shrinks from 1.69uS to 1.22uS - but is that for all calls to the handler? Perhaps 1 in 10 ( 20, 30 ...) calls is still 1.69uS.

MB7
Associate II

@Community member​ 

OK seems I have to go through quite some learning curve here. How can I check the alignment of the Handler?

@S.Ma​ 

I tried that. Did not make a difference at all.

@Community member​ 

The ISR looks like this:

void DMA1_Channel1_IRQHandler(void)
{
 
 
 if(DMA1->ISR & DMA_ISR_TCIF1)  //check we are here cause of a valid interrupt occurred
 {
	DMA1->IFCR |= DMA_IFCR_CTCIF1;	//reset interrupt flag
 
	GPIOC->ODR |= (1U << 14);	//Set Pin high
 
	ev = (v - my_array[0]);
	vp  = A * ev;					
	vi  = B * vi1;			
	if(vi > 4100) vi=4100;					
	if(vi < 0) vi=0;
	vi1 = vi;
	vd  = C * (ev - (e1v+2));			
	e1v = ev;						
	cv = vp + vi + vd;				
	if(cv < 0) cv=0;
	cv_t = cv/2;	
	if(cv_t >  4000 ) cv_t=4000;
 	/*------------------------------------------------------*/
	ei = (my_array[1] - i);
	ip  = D * ei;					
	ii  = E * ii1;			
	if(ii > 4100000 ) ii=4100000;
        if(ii < 0 ) ii=0;
	ii1 = ii;
	id  = F * (ei + (e1i-2));			
	e1i = ei;						
	ci = ip + ii + id;				
	if(ci < 0) ci=0;
	ci_t = ci/1000;					
	if(ci_t >  4000 ) ci_t=4000;
 
	cdac_t = (cv_t - ci_t);
 
	if(cdac_t > 4000) cdac_t=4000;
	if(cdac_t < 1500) cdac_t=1500;
 
	GPIOC->ODR &= ~(1U << 14); //Set Pin low
  
 }
}

All the variables are global. Some of them are "int" and others are "float". I am using the FPU.

The timing shrinks down to 1.22µs for every call to the handler. I verified that with the pulse trigger function of the oscilloscope. No longer pulses occur.

The .MAP file should give a good breakdown of the function placement.

You could perhaps do a listing / disassembly via objcopy or fromelf, and review that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

First thing I would say - Change the setting of the IO pin to use the BSSR register. it is a much safer way of setting the IO pin from an interrupt handler.

Try moving the "... //Set Pin low" before the first "if..." statement - and see if the variation still occurs - assuming it is ok at that point, progressively step/shift the statement to through the handler until the variation occurs. A bit laborious I know, but might help pin point the variation.

S.Ma
Principal

You are using the fpu... in the interrupt routine? If yes, this is a possible warning flag. Variables accessed in the ISR and outside are declared volatile?

MB7
Associate II

This is what I could find in the .map file regarding the DMA1_Channel1_IRQHandler:

 .text          0x0000000008000c88       0x3c /home/MB/opt/stm32CubeIDE_1.10.1/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.linux64_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/thumb/v7e-m+fp/hard/libgcc.a(_fixunsdfdi.o)
                0x0000000008000c88                __aeabi_d2ulz
                0x0000000008000c88                __fixunsdfdi
 *(.text*)
 .text.DMA1_Channel1_IRQHandler
                0x0000000008000cc4      0x258 ./Core/Src/ISR_Handlers.o
                0x0000000008000cc4                DMA1_Channel1_IRQHandler
 .text.cli_cmd_handler_kpv
                0x0000000008000f1c       0x74 ./Core/Src/cli.o
                0x0000000008000f1c                cli_cmd_handler_kpv

And here a few snippets from the .list file that may help to find an issue:

Sections:
Idx Name          Size      VMA       LMA       File off  Algn
  0 .isr_vector   000001d8  08000000  08000000  00010000  2**0
                  CONTENTS, ALLOC, LOAD, READONLY, DATA
  1 .text         00006c0c  080001e0  080001e0  000101e0  2**4
                  CONTENTS, ALLOC, LOAD, READONLY, CODE
  2 .rodata       00000a3c  08006df0  08006df0  00016df0  2**3
                  CONTENTS, ALLOC, LOAD, READONLY, DATA
  3 .ARM.extab    00000000  0800782c  0800782c  000202bc  2**0
                  CONTENTS
  4 .ARM          00000000  0800782c  0800782c  000202bc  2**0
                 CONTENTS	
  5 .preinit_array 00000000  0800782c  0800782c  000202bc  2**0
                  CONTENTS, ALLOC, LOAD, DATA
  6 .init_array   00000004  0800782c  0800782c  0001782c  2**2
                  CONTENTS, ALLOC, LOAD, DATA
  7 .fini_array   00000004  08007830  08007830  00017830  2**2
                  CONTENTS, ALLOC, LOAD, DATA
  8 .data         000002bc  20000000  08007834  00020000  2**2
                  CONTENTS, ALLOC, LOAD, DATA
  9 .bss          000013b8  200002bc  08007af0  000202bc  2**2
                  ALLOC
 10 ._user_heap_stack 00000604  20001674  08007af0  00021674  2**0
                  ALLOC
 11 .ARM.attributes 00000030  00000000  00000000  000202bc  2**0
                  CONTENTS, READONLY
 12 .comment      00000050  00000000  00000000  000202ec  2**0
                  CONTENTS, READONLY
 13 .debug_frame  000017c8  00000000  00000000  0002033c  2**2
                  CONTENTS, READONLY, DEBUGGING, OCTETS
 14 .stab         000000cc  00000000  00000000  00021b04  2**2
                  CONTENTS, READONLY, DEBUGGING
 15 .stabstr      000001b9  00000000  00000000  00021bd0  2**0
                  CONTENTS, READONLY, DEBUGGING

MB7
Associate II
8000cc0:	41f00000 	.word	0x41f00000
 
08000cc4 <DMA1_Channel1_IRQHandler>:
 8000cc4:	4b73      	ldr	r3, [pc, #460]	; (8000e94 <DMA1_Channel1_IRQHandler+0x1d0>)
 8000cc6:	681a      	ldr	r2, [r3, #0]
 8000cc8:	0792      	lsls	r2, r2, #30
 8000cca:	b510      	push	{r4, lr}
 8000ccc:	f140 80c2 	bpl.w	8000e54 <DMA1_Channel1_IRQHandler+0x190>
 8000cd0:	685a      	ldr	r2, [r3, #4]
 8000cd2:	4871      	ldr	r0, [pc, #452]	; (8000e98 <DMA1_Channel1_IRQHandler+0x1d4>)
 8000cd4:	4971      	ldr	r1, [pc, #452]	; (8000e9c <DMA1_Channel1_IRQHandler+0x1d8>)
 8000cd6:	f042 0202 	orr.w	r2, r2, #2
 8000cda:	605a      	str	r2, [r3, #4]
 8000cdc:	4a70      	ldr	r2, [pc, #448]	; (8000ea0 <DMA1_Channel1_IRQHandler+0x1dc>)
 8000cde:	edd1 6a00 	vldr	s13, [r1]
 8000ce2:	6993      	ldr	r3, [r2, #24]
 8000ce4:	f443 4380 	orr.w	r3, r3, #16384	; 0x4000
 8000ce8:	6193      	str	r3, [r2, #24]
 8000cea:	4b6e      	ldr	r3, [pc, #440]	; (8000ea4 <DMA1_Channel1_IRQHandler+0x1e0>)
 8000cec:	681a      	ldr	r2, [r3, #0]
 8000cee:	8803      	ldrh	r3, [r0, #0]
 8000cf0:	b29b      	uxth	r3, r3
 8000cf2:	1ad2      	subs	r2, r2, r3
 8000cf4:	4b6c      	ldr	r3, [pc, #432]	; (8000ea8 <DMA1_Channel1_IRQHandler+0x1e4>)
 8000cf6:	601a      	str	r2, [r3, #0]
 8000cf8:	4b6c      	ldr	r3, [pc, #432]	; (8000eac <DMA1_Channel1_IRQHandler+0x1e8>)
 8000cfa:	681b      	ldr	r3, [r3, #0]
 8000cfc:	4353      	muls	r3, r2
 8000cfe:	ee07 3a90 	vmov	s15, r3
 8000d02:	4b6b      	ldr	r3, [pc, #428]	; (8000eb0 <DMA1_Channel1_IRQHandler+0x1ec>)
 8000d04:	eef8 7ae7 	vcvt.f32.s32	s15, s15
 8000d08:	edc3 7a00 	vstr	s15, [r3]
 8000d0c:	4b69      	ldr	r3, [pc, #420]	; (8000eb4 <DMA1_Channel1_IRQHandler+0x1f0>)
 8000d0e:	681b      	ldr	r3, [r3, #0]
 8000d10:	4353      	muls	r3, r2
 8000d12:	ee07 3a10 	vmov	s14, r3
 8000d16:	eeb8 7ac7 	vcvt.f32.s32	s14, s14
 8000d1a:	4b67      	ldr	r3, [pc, #412]	; (8000eb8 <DMA1_Channel1_IRQHandler+0x1f4>)
 8000d1c:	ee37 7a26 	vadd.f32	s14, s14, s13
 8000d20:	eddf 6a66 	vldr	s13, [pc, #408]	; 8000ebc <DMA1_Channel1_IRQHandler+0x1f8>
 8000d24:	eeb4 7ae6 	vcmpe.f32	s14, s13
 8000d28:	eef1 fa10 	vmrs	APSR_nzcv, fpscr
 8000d2c:	f340 8093 	ble.w	8000e56 <DMA1_Channel1_IRQHandler+0x192>
 8000d30:	edc3 6a00 	vstr	s13, [r3]
 8000d34:	edd3 6a00 	vldr	s13, [r3]
 8000d38:	4c61      	ldr	r4, [pc, #388]	; (8000ec0 <DMA1_Channel1_IRQHandler+0x1fc>)
 8000d3a:	edc1 6a00 	vstr	s13, [r1]
 8000d3e:	4961      	ldr	r1, [pc, #388]	; (8000ec4 <DMA1_Channel1_IRQHandler+0x200>)
 8000d40:	6824      	ldr	r4, [r4, #0]
 8000d42:	680b      	ldr	r3, [r1, #0]
 8000d44:	600a      	str	r2, [r1, #0]
 8000d46:	1ad3      	subs	r3, r2, r3
 8000d48:	4363      	muls	r3, r4
 8000d4a:	ee07 3a10 	vmov	s14, r3
 8000d4e:	ee77 7aa6 	vadd.f32	s15, s15, s13
 8000d52:	eeb8 7ac7 	vcvt.f32.s32	s14, s14
 8000d56:	4b5c      	ldr	r3, [pc, #368]	; (8000ec8 <DMA1_Channel1_IRQHandler+0x204>)
 8000d58:	4a5c      	ldr	r2, [pc, #368]	; (8000ecc <DMA1_Channel1_IRQHandler+0x208>)
 8000d5a:	ed83 7a00 	vstr	s14, [r3]
 8000d5e:	ee77 7a87 	vadd.f32	s15, s15, s14
 8000d62:	495b      	ldr	r1, [pc, #364]	; (8000ed0 <DMA1_Channel1_IRQHandler+0x20c>)
 8000d64:	eefd 7ae7 	vcvt.s32.f32	s15, s15
 8000d68:	ee17 3a90 	vmov	r3, s15
 8000d6c:	2b00      	cmp	r3, #0
 8000d6e:	bfb8      	it	lt
 8000d70:	2300      	movlt	r3, #0
 8000d72:	6013      	str	r3, [r2, #0]
 8000d74:	6813      	ldr	r3, [r2, #0]
 8000d76:	8842      	ldrh	r2, [r0, #2]
 8000d78:	4856      	ldr	r0, [pc, #344]	; (8000ed4 <DMA1_Channel1_IRQHandler+0x210>)
 8000d7a:	f5b3 6f7a 	cmp.w	r3, #4000	; 0xfa0
 8000d7e:	bfc8      	it	gt
 8000d80:	f44f 637a 	movgt.w	r3, #4000	; 0xfa0
 8000d84:	600b      	str	r3, [r1, #0]
 8000d86:	4b54      	ldr	r3, [pc, #336]	; (8000ed8 <DMA1_Channel1_IRQHandler+0x214>)
 8000d88:	edd0 6a00 	vldr	s13, [r0]
 8000d8c:	681b      	ldr	r3, [r3, #0]
 8000d8e:	b292      	uxth	r2, r2
 8000d90:	1ad2      	subs	r2, r2, r3
 8000d92:	4b52      	ldr	r3, [pc, #328]	; (8000edc <DMA1_Channel1_IRQHandler+0x218>)
 8000d94:	601a      	str	r2, [r3, #0]
 8000d96:	4b52      	ldr	r3, [pc, #328]	; (8000ee0 <DMA1_Channel1_IRQHandler+0x21c>)
 8000d98:	681b      	ldr	r3, [r3, #0]
 8000d9a:	4353      	muls	r3, r2
 8000d9c:	ee07 3a90 	vmov	s15, r3
 8000da0:	4b50      	ldr	r3, [pc, #320]	; (8000ee4 <DMA1_Channel1_IRQHandler+0x220>)
 8000da2:	eef8 7ae7 	vcvt.f32.s32	s15, s15
 8000da6:	edc3 7a00 	vstr	s15, [r3]
 8000daa:	4b4f      	ldr	r3, [pc, #316]	; (8000ee8 <DMA1_Channel1_IRQHandler+0x224>)
 8000dac:	681b      	ldr	r3, [r3, #0]
 8000dae:	4353      	muls	r3, r2
 8000db0:	ee07 3a10 	vmov	s14, r3
 8000db4:	eeb8 7ac7 	vcvt.f32.s32	s14, s14
 8000db8:	4b4c      	ldr	r3, [pc, #304]	; (8000eec <DMA1_Channel1_IRQHandler+0x228>)
 8000dba:	ee37 7a26 	vadd.f32	s14, s14, s13
 8000dbe:	eddf 6a4c 	vldr	s13, [pc, #304]	; 8000ef0 <DMA1_Channel1_IRQHandler+0x22c>
 8000dc2:	eeb4 7ae6 	vcmpe.f32	s14, s13
 8000dc6:	eef1 fa10 	vmrs	APSR_nzcv, fpscr
 8000dca:	dd50      	ble.n	8000e6e <DMA1_Channel1_IRQHandler+0x1aa>
 8000dcc:	edc3 6a00 	vstr	s13, [r3]
 8000dd0:	edd3 6a00 	vldr	s13, [r3]
 8000dd4:	4c47      	ldr	r4, [pc, #284]	; (8000ef4 <DMA1_Channel1_IRQHandler+0x230>)
 8000dd6:	edc0 6a00 	vstr	s13, [r0]
 8000dda:	4847      	ldr	r0, [pc, #284]	; (8000ef8 <DMA1_Channel1_IRQHandler+0x234>)
 8000ddc:	6824      	ldr	r4, [r4, #0]
 8000dde:	6803      	ldr	r3, [r0, #0]
 8000de0:	6002      	str	r2, [r0, #0]
 8000de2:	1ad3      	subs	r3, r2, r3
 8000de4:	4363      	muls	r3, r4
 8000de6:	ee07 3a10 	vmov	s14, r3
 8000dea:	ee77 7aa6 	vadd.f32	s15, s15, s13
 8000dee:	eeb8 7ac7 	vcvt.f32.s32	s14, s14
 8000df2:	4b42      	ldr	r3, [pc, #264]	; (8000efc <DMA1_Channel1_IRQHandler+0x238>)
 8000df4:	4a42      	ldr	r2, [pc, #264]	; (8000f00 <DMA1_Channel1_IRQHandler+0x23c>)
 8000df6:	ed83 7a00 	vstr	s14, [r3]
 8000dfa:	ee77 7a87 	vadd.f32	s15, s15, s14
 8000dfe:	eefd 7ae7 	vcvt.s32.f32	s15, s15
 8000e02:	ee17 3a90 	vmov	r3, s15
 8000e06:	2b00      	cmp	r3, #0
 8000e08:	bfb8      	it	lt
 8000e0a:	2300      	movlt	r3, #0
 8000e0c:	6013      	str	r3, [r2, #0]
 8000e0e:	6813      	ldr	r3, [r2, #0]
 8000e10:	4a3c      	ldr	r2, [pc, #240]	; (8000f04 <DMA1_Channel1_IRQHandler+0x240>)
 8000e12:	4293      	cmp	r3, r2
 8000e14:	4a3c      	ldr	r2, [pc, #240]	; (8000f08 <DMA1_Channel1_IRQHandler+0x244>)
 8000e16:	bfce      	itee	gt
 8000e18:	f44f 637a 	movgt.w	r3, #4000	; 0xfa0
 8000e1c:	f44f 707a 	movle.w	r0, #1000	; 0x3e8
 8000e20:	fb93 f3f0 	sdivle	r3, r3, r0
 8000e24:	6013      	str	r3, [r2, #0]
 8000e26:	6812      	ldr	r2, [r2, #0]
 8000e28:	680b      	ldr	r3, [r1, #0]
 8000e2a:	1a9b      	subs	r3, r3, r2
 8000e2c:	f5b3 6f7a 	cmp.w	r3, #4000	; 0xfa0
 8000e30:	4a36      	ldr	r2, [pc, #216]	; (8000f0c <DMA1_Channel1_IRQHandler+0x248>)
 8000e32:	dd28      	ble.n	8000e86 <DMA1_Channel1_IRQHandler+0x1c2>
 8000e34:	f44f 637a 	mov.w	r3, #4000	; 0xfa0
 8000e38:	6013      	str	r3, [r2, #0]
 8000e3a:	4b35      	ldr	r3, [pc, #212]	; (8000f10 <DMA1_Channel1_IRQHandler+0x24c>)
 8000e3c:	6819      	ldr	r1, [r3, #0]
 8000e3e:	6813      	ldr	r3, [r2, #0]
 8000e40:	4a34      	ldr	r2, [pc, #208]	; (8000f14 <DMA1_Channel1_IRQHandler+0x250>)
 8000e42:	ea43 5301 	orr.w	r3, r3, r1, lsl #20
 8000e46:	65d3      	str	r3, [r2, #92]	; 0x5c
 8000e48:	f102 4278 	add.w	r2, r2, #4160749568	; 0xf8000000
 8000e4c:	6993      	ldr	r3, [r2, #24]
 8000e4e:	f043 4380 	orr.w	r3, r3, #1073741824	; 0x40000000
 8000e52:	6193      	str	r3, [r2, #24]
 8000e54:	bd10      	pop	{r4, pc}
 8000e56:	eeb5 7ac0 	vcmpe.f32	s14, #0.0
 8000e5a:	eddf 6a2f 	vldr	s13, [pc, #188]	; 8000f18 <DMA1_Channel1_IRQHandler+0x254>
 8000e5e:	eef1 fa10 	vmrs	APSR_nzcv, fpscr
 8000e62:	bf48      	it	mi
 8000e64:	eeb0 7a66 	vmovmi.f32	s14, s13
 8000e68:	ed83 7a00 	vstr	s14, [r3]
 8000e6c:	e762      	b.n	8000d34 <DMA1_Channel1_IRQHandler+0x70>
 8000e6e:	eeb5 7ac0 	vcmpe.f32	s14, #0.0
 8000e72:	eddf 6a29 	vldr	s13, [pc, #164]	; 8000f18 <DMA1_Channel1_IRQHandler+0x254>
 8000e76:	eef1 fa10 	vmrs	APSR_nzcv, fpscr
 8000e7a:	bf48      	it	mi
 8000e7c:	eeb0 7a66 	vmovmi.f32	s14, s13
 8000e80:	ed83 7a00 	vstr	s14, [r3]
 8000e84:	e7a4      	b.n	8000dd0 <DMA1_Channel1_IRQHandler+0x10c>
 8000e86:	f240 51db 	movw	r1, #1499	; 0x5db
 8000e8a:	428b      	cmp	r3, r1
 8000e8c:	bfd8      	it	le
 8000e8e:	f240 53dc 	movwle	r3, #1500	; 0x5dc
 8000e92:	e7d1      	b.n	8000e38 <DMA1_Channel1_IRQHandler+0x174>
 8000e94:	40020000 	.word	0x40020000
 8000e98:	20001548 	.word	0x20001548
 8000e9c:	20001544 	.word	0x20001544
 8000ea0:	48000800 	.word	0x48000800
 8000ea4:	20001550 	.word	0x20001550
 8000ea8:	20001524 	.word	0x20001524
 8000eac:	200000cc 	.word	0x200000cc
 8000eb0:	2000154c 	.word	0x2000154c
 8000eb4:	200000c4 	.word	0x200000c4
 8000eb8:	20001540 	.word	0x20001540
 8000ebc:	45802000 	.word	0x45802000
 8000ec0:	200014f8 	.word	0x200014f8
 8000ec4:	2000151c 	.word	0x2000151c
 8000ec8:	2000153c 	.word	0x2000153c
 8000ecc:	20001508 	.word	0x20001508
 8000ed0:	2000150c 	.word	0x2000150c
 8000ed4:	20001530 	.word	0x20001530
 8000ed8:	20001538 	.word	0x20001538
 8000edc:	20001520 	.word	0x20001520
 8000ee0:	200000c8 	.word	0x200000c8
 8000ee4:	20001534 	.word	0x20001534
 8000ee8:	200000c0 	.word	0x200000c0
 8000eec:	2000152c 	.word	0x2000152c
 8000ef0:	4a7a3e80 	.word	0x4a7a3e80
 8000ef4:	200014f4 	.word	0x200014f4
 8000ef8:	20001518 	.word	0x20001518
 8000efc:	20001528 	.word	0x20001528
 8000f00:	20001500 	.word	0x20001500
 8000f04:	003d0ce7 	.word	0x003d0ce7
 8000f08:	20001504 	.word	0x20001504
 8000f0c:	200014fc 	.word	0x200014fc
 8000f10:	200000d0 	.word	0x200000d0
 8000f14:	50000800 	.word	0x50000800
 8000f18:	00000000 	.word	0x00000000
 
08000f1c <cli_cmd_handler_kpv>:
 8000f1c:	2802      	cmp	r0, #2