2025-04-07 6:40 PM
I want to write a program for a fresh (first time power applied to it so there is nothing in Flash) STM32G0B1 that executes in RAM, resets the nBOOT_SEL bit in the Option Bytes (to allow DFU Mode to be invoked when Flash has been written).
The reason why I want to execute in RAM is to avoid having to run a program that is loaded in Flash (and resets nBOOT_SEL as discussed above) which is loaded into Flash that requires a power cycle to restart so that DFU Mode can be enabled in the MCU to load the actual product firmware.
This is being done in manufacturing test, so avoiding a power cycle (which takes about a minute due to other hardware in the application) would be of advantage.
Could anybody point me to:
I think the last two links for creating a program that runs in SRAM are probably closest to what I want to do but I'm hoping that there is a crisp explanation that I can follow.
For resetting the nBOOL_SEL bit, I'm going to use the following guide (with standard STM/HAL development tools/libraries):
https://community.st.com/t5/stm32-mcus/how-to-program-stm32-option-bytes-with-the-hal-api/ta-p/49660
Any comments or suggestions are most welcome!
myke
2025-04-16 10:29 PM
I wanted to follow up with this - I've got an application running that resets the nBOOT_SEL bit but now I need to get it running in SRAM after being loaded into the STM32G0B1RET6 MCU using DFU.
First I created a simple application to Flash an LED on the test board, I created a .bin version of it and loaded it using DFU:
As you can see in the screenshot above, the download takes place without issue.
The only problem I have is that the code won't start executing after I load it - I have tried adding the ":leave" modifier but no joy. If I reset the board, the code works fine with the LED flashing as expected.
---
For testing in SRAM, I fully erase the MCU to make sure I don't get any unexpected results from a previous Flash load.
I created a new project with the same main.c as the first case but with the following changes:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20002000, LENGTH = 144K
FLASH (rx) : ORIGIN = 0x20000000, LENGTH = 512K
}I then attach S-Link, connect (without touching anything on the board including power or the USB cable) and look at the contents of SRAM and see:
So, the immediate issues I see here are:
So, any ideas?
@clkr , I've seen your post and, I'm not disabling the interrupts used by DFU - I think this explains why the Flashed version doesn't start (I've tried it with both with and without the ":leave" Modifier to the "-s" dfu-util option.
Thanx - I feel like it's something simple but I really can't figure out what I'm doing wrong.
myke