cancel
Showing results for 
Search instead for 
Did you mean: 

How can I transmit a UART message using a SMT32G474 B-G474E-DPOW1

LChin.1
Associate

I am not new to working with STM32 MCUs but this is a one-of-one.

I have checked the baud rate to 115200 with 8E1, the serial com port driver is showing up on my computer and when I measure the USART-TX pin using an oscilloscope it is showing a signal. I am not getting any errors.

This said however, there is nothing showing up on my teraterm terminal or termite terminal, I am open to suggestions, been trying to fix this all day :)

2 REPLIES 2
gbm
Lead III

Why not 115200 8 N 1 ?

ST-Link VCOM is not a complete implementation of CDC ACM. It may not support some features/options.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
MM..1
Chief III

G474 have 3 USART and variants for pin for every signal. Only one is connected to VCOM on debuger bridge.

You dont explain what you scope and ...