2018-11-07 11:10 AM
I am new to Atollic TrueStudio V9.1.0 on Win XP Pro SP3. I can create and build new project but Debug does nothing. I do not see the Binaries folder in the Project window. How and when and where does the Binaries folder get created?
2018-11-09 06:34 AM
Hi @mandrake ,
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-11-09 10:15 AM
Thanks for the suggestions. I tried both. No joy.
Here is the build command.
13:03:23 **** Rebuild of configuration Debug for project Project001 ****
Info: Internal Builder is used for build
arm-atollic-eabi-gcc -c ..\Libraries\STM32F4xx_StdPeriph_Driver\src\stm32f4xx_pwr.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DSTM32F4XX -DSTM32F40XX -DUSE_STDPERIPH_DRIVER -I../src -I../Libraries/CMSIS/Include -I../Libraries/Device/STM32F4xx/Include -I../Libraries/STM32F4xx_StdPeriph_Driver/inc -O0 -ffunction-sections -fdata-sections -g -fstack-usage -Wall -specs=nano.specs -o Libraries\STM32F4xx_StdPeriph_Driver\src\stm32f4xx_pwr.o
13:03:23 Build Finished (took 204ms)
Can you spot what is missing that prevents the Binaries folder from being created?
2018-11-09 10:26 AM
btw, how did that university name appear in my forum ID instead of the preferred Community Member?
How can I change my forum ID?