2023-07-25 6:00 PM - edited 2023-07-25 6:03 PM
I had an unattended script to regenerate and compile the project.
In it, I call CubeMX using this cmd:
java.exe -jar STM32CubeMX.jar -q cubemx_script
These are the contents of cubemx_script:
config load myProject.ioc
project generate
exit
It has worked perfectly for more than a year. With 1.13.0, it no longer works.
I can see this in the CubeMX window:
config load myProject.ioc
2023-07-26 02:48:57,629 [INFO] JxBrowserEngine:151 - Initiate JxBrowser Engine with user profile folder
2023-07-26 02:48:57,670 [INFO] MicroXplorer:468 - Change Database Path :
2023-07-26 02:48:57,671 [INFO] MicroXplorer:498 - Change Database Version : DB.6.0.90
2023-07-26 02:48:57,674 [WARN] ThirdParty:871 - waiting for thirdparty lock release [close project]
2023-07-26 02:48:57,708 [ERROR] JxBrowserEngine:69 - Can't initiate JxBrowser engine com.teamdev.jxbrowser.engine.ChromiumBinariesExtractionException: Failed to extract Chromium binaries into C:\Users\David\.stm32cubemx\.jxbrowser-7.30.2\Chromium
Exception in thread "Thread-2" java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at com.st.microxplorer.plugins.userauth.UserAuth.activatePlugin(UserAuth.java:200)
at com.st.microxplorer.maingui.MainFrame.lambda$initialization$0(MainFrame.java:189)
at java.base/java.lang.Thread.run(Thread.java:833)
Not sure why is it trying to extract Chromium binaries or why is it failing.
I'll stay wih 1.12.1 for now.
2023-07-28 8:56 AM
Hello @DavidAlfa
First let me thank you for posting.
I try to compile and regenerate a project with this cmd :
jre\bin\java -jar STM32CubeMX.exe -s C:\Temp\cubemx_script.txtI just add the path of the project in the script :
config load C:\STM32CubeProjects\myProject\myProject.ioc
project generate
exitand it worked correctly, keep using 1.13.0 version and try to make sure of the right path of your project.
thank you
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.