Integrated jxBrowser not working
Hi there,
after installing STM32CubeIDE for the first time I cannot get it up and running.
When I open any window which seems to rely on the included jxbrowser nothing happens.
This prevents me from logging into my ST Account, viewing the Information center, opening the "Manage embbeded software packages" window and so on.
As soon as I executed one of the actions above errors are generated in the logfiles (see attached below).
I am running a Linux VM with the following specs:
Linux VM-Kubuntu-23 6.5.0-26-generic #26-Ubuntu SMP PREEMPT_DYNAMIC Tue Mar 5 21:19:28 UTC 2024 x86_64 x86_64
x86_64 GNU/Linux
I tried installing and reinstalling versions 1.14 and 1.15 with the same outcome and problem every time.
I tried using the Debian and generic Linux version with the same outcome and problem every time.
Is there anything I can do to work around this bug?
Isolated error from .ide.log:
2024-03-28 16:32:04,078 [INFO] JxBrowserEngine:152 - Initiate JxBrowser Engine with user profile folder
2024-03-28 16:32:04,219 [INFO] CheckServerUpdateThread:120 - End of CheckServer Thread
2024-03-28 16:32:04,531 [ERROR] JxBrowserEngine:70 - Can't initiate JxBrowser engine com.teamdev.jxbrowser.engine.ChromiumBinariesDeliveryException: com.teamdev.jxbrowser.engine.ChromiumBinariesDeliveryException: Failed to extract Chromium binaries into /home/vincent/.stm32cubeide/.jxbrowser-7.35.1/Chromium
Isolated error from .log:
!SESSION 2024-03-28 16:31:54.821 -----------------------------------------------
eclipse.buildId=Version 1.14.0
java.version=17.0.8.1
java.vendor=Eclipse Adoptium
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Command-line arguments: -os linux -ws gtk -arch x86_64
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 4 4 2024-03-28 16:31:59.525
!MESSAGE CubeMX plugin appears to be active, Log4j initialization might be too late.
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 1 1 2024-03-28 16:31:59.526
!MESSAGE Log4j2 initialized with config file /home/vincent/STM32CubeIDE/workspace_1.14.0/.metadata/.log4j2.xml
!ENTRY com.st.stm32cube.ide.mcu.ide 1 1 2024-03-28 16:32:01.491
!MESSAGE Started RMI Server, listening on port 41337
!ENTRY org.eclipse.ui.workbench 4 2 2024-03-28 16:32:04.532
!MESSAGE Problems occurred when invoking code from plug-in: "org.eclipse.ui.workbench".
!STACK 0
java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at com.st.microxplorer.plugins.userauth.UserAuth.activatePlugin(UserAuth.java:201)
at com.st.stm32cube.common.mx.userauth.UserAuthAdapter.<init>(UserAuthAdapter.java:29)
at com.st.stm32cube.common.mx.userauth.UserAuthProvider.getUserAuthAdapter(UserAuthProvider.java:16)
at com.st.stm32cube.common.ecosystemintegration.ui.core.MCUEcoSystemIntegrationUiHelper.getUserAuth(MCUEcoSystemIntegrationUiHelper.java:100)
at com.st.stm32cube.ide.mcu.userauth.UserAuthStartup.earlyStartup(UserAuthStartup.java:41)
at org.eclipse.ui.internal.EarlyStartupRunnable.runEarlyStartup(EarlyStartupRunnable.java:79)
at org.eclipse.ui.internal.EarlyStartupRunnable.run(EarlyStartupRunnable.java:55)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.ui.internal.Workbench$39.run(Workbench.java:2737)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
!ENTRY org.eclipse.ui 4 0 2024-03-28 16:32:04.532
!MESSAGE Unable to execute early startup code for the org.eclipse.ui.IStartup extension contributed by the 'com.st.stm32cube.ide.mcu.ide' plug-in.
!STACK 0
java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at com.st.microxplorer.plugins.userauth.UserAuth.activatePlugin(UserAuth.java:201)
at com.st.stm32cube.common.mx.userauth.UserAuthAdapter.<init>(UserAuthAdapter.java:29)
at com.st.stm32cube.common.mx.userauth.UserAuthProvider.getUserAuthAdapter(UserAuthProvider.java:16)
at com.st.stm32cube.common.ecosystemintegration.ui.core.MCUEcoSystemIntegrationUiHelper.getUserAuth(MCUEcoSystemIntegrationUiHelper.java:100)
at com.st.stm32cube.ide.mcu.userauth.UserAuthStartup.earlyStartup(UserAuthStartup.java:41)
at org.eclipse.ui.internal.EarlyStartupRunnable.runEarlyStartup(EarlyStartupRunnable.java:79)
at org.eclipse.ui.internal.EarlyStartupRunnable.run(EarlyStartupRunnable.java:55)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.ui.internal.Workbench$39.run(Workbench.java:2737)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
!ENTRY org.eclipse.e4.ui.workbench 4 0 2024-03-28 16:32:37.912
!MESSAGE Command 'com.st.stm32cube.ide.mcu.ide.command.userAuth.login' failed
!STACK 0
org.eclipse.core.commands.ExecutionException: Error executing 'com.st.stm32cube.ide.mcu.ide.command.userAuth.login': java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at org.eclipse.e4.core.commands.internal.HandlerServiceHandler.execute(HandlerServiceHandler.java:170)
at org.eclipse.core.commands.Command.executeWithChecks(Command.java:488)
at org.eclipse.core.commands.ParameterizedCommand.executeWithChecks(ParameterizedCommand.java:485)
at org.eclipse.e4.core.commands.internal.HandlerServiceImpl.executeHandler(HandlerServiceImpl.java:213)
at org.eclipse.e4.ui.workbench.renderers.swt.HandledContributionItem.executeItem(HandledContributionItem.java:438)
at org.eclipse.e4.ui.workbench.renderers.swt.AbstractContributionItem.handleWidgetSelection(AbstractContributionItem.java:449)
at org.eclipse.e4.ui.workbench.renderers.swt.AbstractContributionItem.lambda$2(AbstractContributionItem.java:475)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5855)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1529)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5065)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4517)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1155)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:342)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1046)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:645)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:342)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:552)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:171)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:651)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:588)
at org.eclipse.equinox.launcher.Main.run(Main.java:1459)
at org.eclipse.equinox.launcher.Main.main(Main.java:1432)
Caused by: org.eclipse.e4.core.di.InjectionException: java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:68)
at org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:300)
at org.eclipse.e4.core.internal.di.InjectorImpl.invoke(InjectorImpl.java:234)
at org.eclipse.e4.core.contexts.ContextInjectionFactory.invoke(ContextInjectionFactory.java:173)
at org.eclipse.e4.core.commands.internal.HandlerServiceHandler.execute(HandlerServiceHandler.java:156)
... 33 more
Caused by: java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
at com.st.microxplorer.plugins.userauth.UserAuth.activatePlugin(UserAuth.java:201)
at com.st.stm32cube.common.mx.userauth.UserAuthAdapter.<init>(UserAuthAdapter.java:29)
at com.st.stm32cube.common.mx.userauth.UserAuthProvider.getUserAuthAdapter(UserAuthProvider.java:16)
at com.st.stm32cube.common.ecosystemintegration.ui.core.MCUEcoSystemIntegrationUiHelper.getUserAuth(MCUEcoSystemIntegrationUiHelper.java:100)
at com.st.stm32cube.ide.mcu.userauth.UserAuth.execute(UserAuth.java:43)
at org.eclipse.ui.internal.handlers.HandlerProxy.execute(HandlerProxy.java:283)
at org.eclipse.ui.internal.handlers.E4HandlerProxy.execute(E4HandlerProxy.java:97)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58)
... 37 more
Let me know if a full log is needed.