2018-11-07 6:25 AM
Hi. After many hours my stm32f091 board does not receive what I send to it using uart.
Please could someone confirm that I'm using uart, rx and dma correctly?
So this is my sequence:
CubeMX -> usart1 -> DMA Settings -> add
(on RX, circular, memory)
Usart1 global interrupt: checked
main.c
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
bool ReadyRead0= false;
std::vector<unsigned char> VBufferSerial0Read;
unsigned char MicroBufferSerial0Read[2];
unsigned long LastByteIn0;
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
if (huart->Instance== USART1) {
VBufferSerial0Read.push_back(MicroBufferSerial0Read[0]);
LastByteIn0= HAL_GetTick();
ReadyRead0= true;
}
}
/* USER CODE END PFP */
int main(void)
{
HAL_UART_Receive_DMA(&huart1, (uint8_t*)&MicroBufferSerial0Read, 1);
for(;;) {
if (ReadyRead0) {
......
......
......
ReadyRead0= false;
}
}
}
2018-11-07 6:46 AM
There should be an example in your device firmware package. You are not checking what the HAL returns. whats happening in your debug...
2018-11-07 6:52 AM
Yes you should as @randy2 says you should check what happening in your debug
2018-11-07 11:16 PM
Is my code ok? Is there a better way to use dma on rx channel, without to know how many bytes are coming?
2018-11-08 5:08 AM
Hi there,
Yes you can use IDLE interrupts in normal mode, not circular. The was a good example of code if you google "Efficiently receive UART data using DMA"
2018-11-08 5:42 AM
Excellent work, Tick, Tick Tick....
my sequence:
CubeMX -> usart1 -> DMA Settings -> add
(on RX, circular, memory)
Usart1 global interrupt: checkedthis is the Polling method..
In your process, are you waiting for a byte or a length ?
either way, you can Peek inside the RxDMAbuffer without reading it..
that is, if you are waiting for a length or sequence set.. You can Peek without touching
Usually a buffer has PtrIN and PtrOUT
on startup
PtrIN =0; // not needed
PtrOUT =0; // needed
if PtrIN - PtrOUT =0, there is no data in the buffer...
If the DMA receives a byte, PtrIN is calculated from the DMAbufferPointer.
U1RxBufferPtrIN = U1RxBufSize - huart2.hdmarx->Instance->CNDTR;used here to check the UNread length of the buffer
char readableU1(void) {
U1RxBufferPtrIN = U1RxBufSize - huart2.hdmarx->Instance->CNDTR;
return U1RxBufferPtrIN - U1RxBufferPtrOUT; //UNread length
}I had to initialise the Rx interrupt, but I dont use the callback.
char readU1(void) {
char readByte = Usart1RxDMABuffer[U1RxBufferPtrOUT++];
if (U1RxBufferPtrOUT >= U1RxBufSize) U1RxBufferPtrOUT = 0;
return readByte;
}
2018-11-09 8:55 AM
Your approach is very interesting.
I have just applied it and started to test.
I hope my demo board will work correctly till monday.
Have a nice weekend.