2021-12-17 2:17 AM
2021-12-17 3:45 AM
Is this a custom board?
Are any of the queries to the eMMC chip illiciting a response?
Clocks, PLLs, Pins, Power?
2021-12-17 6:50 AM
What clock rate are you using? Might try slowing it down by an order of magnitude to see if results change. If so, the culprit is likely the slow and poorly done HAL eMMC library.
2021-12-17 6:57 AM
Hi @Community member,
Thanks for your answer
It is a Geenliant GLS85VM1507 Board.
The first command gives response when I cup the power and put it back but the second one never give response
Everything is fine for the clocks, PLLs, Pins and power.
2021-12-17 7:35 AM
That sounds like a CHIP, not a BOARD
If GreenLiant made the board, have them provide working reference code.
>>Everything is fine for the clocks, PLLs, Pins and power.
Yet not work properly. My approach to this is to unpack all the RCC PLL,SDMMC clock tree settings so I know which source is used and how fast the clock to the part is.
I'd start proving it works a 25-MHz in 1-bit mode, and walk my way up to 4 and 8-bit operation, and then up to 50/52 MHz and DDR modes.
Review the schematics, double checking pull up and series resistors placed, and supplies to the part.
Not sure screen shots of library code are the path to success here.
2021-12-17 7:49 AM
2021-12-17 7:50 AM
2021-12-17 7:50 AM
Maybe you can see the problem with that.
Thanks for your answer
2021-12-17 8:00 AM
2021-12-17 8:02 AM
With the .ioc file, you can see my clock config.