2021-06-16 7:18 AM
On the the disco board it is set up as follows:-
/**QUADSPI GPIO Configuration
PE2 ------> QUADSPI_BK1_IO2
PB6 ------> QUADSPI_BK1_NCS
PC10 ------> QUADSPI_BK1_IO1
PC9 ------> QUADSPI_BK1_IO0
PB2 ------> QUADSPI_CLK
PD13 ------> QUADSPI_BK1_IO3
On the custom board I've had to change PD13 to PA1 (AF9) for the IO3 line in HAL_QSPI_MspInit() but I can still see the data being sent on PD13? There was no data on PA1.
Thanks,
Will.
Solved! Go to Solution.
2021-06-16 7:34 AM
Perhaps use the debugger and double check the RCC, and GPIO pin configurations
Check you aren't pulling in some different code, or that it is linking the BSP, perhaps due to WEAK linkage.
Look at a listing file, see what codes actually bound.
Show the actual code.
2021-06-16 7:34 AM
Perhaps use the debugger and double check the RCC, and GPIO pin configurations
Check you aren't pulling in some different code, or that it is linking the BSP, perhaps due to WEAK linkage.
Look at a listing file, see what codes actually bound.
Show the actual code.
2021-06-17 3:01 AM
Hi @WScot.1 ,
As guessed by Tesla: most probably you still use BSP drivers which are specific to ST discovery board with your custom board, then your GPIO configuration is overwritten by the one used in the BSP.
Try to get rid of these drivers in your application while using your own PCB.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-18 2:13 AM
Many thanks to both for your help. I'm still working on the issue and one thing that we've changed is instead of using the flash chip MX25L51245G in 8-pin configuration (8-WSON) we're using 16-pin package (16-PIN SOP). I though the shared reset#/SI03 might be an issue for the new memory chip so tried
configuring the quadspi in dual mode, but still have verification of external flash failing. I'm now wondering if we need to write our own external loader to accommodate the new memory chip?
Thanks Will.
2021-06-18 10:25 AM
You'd need a modified loader to account for the different pin usage, and program the memory via ST-LINK, etc.
I don't have a PA1 variant, but could likely fashion one
https://github.com/cturvey/stm32extldr/tree/main/f7_mx25l512g
2021-06-18 7:40 PM
2021-06-21 1:11 AM
Great, thanks Tesla, I did work on one myself last week which I'm about to test, but I will try yours out too.
Thanks again, Will.
2021-06-25 4:33 AM
Thanks for your help, I now have a working flash loader using PA1 for IO3.