2020-12-04 11:25 PM
2020-12-05 09:17 AM
Pull BOOT0 low to ensure it measures as VIL as the supply rises.
Entering the loader suggests it sees VIH
2020-12-05 02:10 AM
That is in the bootloader. How is the BOOT0 pin set?
JW
2020-12-05 03:38 AM
BOOT0 pin is not connected anywhere. It is left idle.
2020-12-05 04:43 AM
AN2586 section 3. Which binary level does a floating pin have?
2020-12-05 08:57 AM
BOOT1 is not available. BOOT0 is left floating.
When power supply is given, at BOOT0 pin , a high pulse is observed with 1.6V, 5.4ms. The snapshot is attached.
Will it cause any bootloader issue?
2020-12-05 09:17 AM
Pull BOOT0 low to ensure it measures as VIL as the supply rises.
Entering the loader suggests it sees VIH
2020-12-08 08:37 AM
System Reset works fine now after pulling Boot0 pin lo low.
Thanks everyone for your help!!