cancel
Showing results for 
Search instead for 
Did you mean: 

hi i am using NUCLEOG0B1RE development board. i am not able to debug the code on keil ide as the ide abruptly closed but the program is running fine on stmcubeide. can anyone suggest what could be the problem

SSING.31
Associate II
 
3 REPLIES 3
Imen.D
ST Employee

Hello @SSING.3​,

Have you an Error message? Can you access the device via STM32CubeProgrammer?

Do you have the same problem with any other boards?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
SSING.31
Associate II

no i am not getting any error message as soon as i select st-link option in debugger and run keil ide closed. while in cubeide it runs fine. does any setting i need to do in keil ide for nucleog0b1re board.

SSING.31
Associate II

i am not able to download the code in flash as it crash there only and it is running fne with cubeprogrammer.