2023-01-12 2:54 AM
2023-01-12 4:44 AM
Hello @SSING.3,
Have you an Error message? Can you access the device via STM32CubeProgrammer?
Do you have the same problem with any other boards?
Imen
2023-01-12 8:42 PM
no i am not getting any error message as soon as i select st-link option in debugger and run keil ide closed. while in cubeide it runs fine. does any setting i need to do in keil ide for nucleog0b1re board.
2023-01-12 10:14 PM
i am not able to download the code in flash as it crash there only and it is running fne with cubeprogrammer.