cancel
Showing results for 
Search instead for 
Did you mean: 

hey i want to read a temperature sensor and a humidity sensor i want to send the values via cdc to my pc and then read them in c# windows forms my question is now how can i read two adc at the same time so i have separate data ? here you have my stm code

MSchmutz
Associate II

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

  HAL_ADC_Start(&hadc2);

  HAL_ADC_Start(&hadc1);

if (HAL_ADC_PollForConversion(&hadc2, 10) == HAL_OK)

{

 adcValTemp = HAL_ADC_GetValue(&hadc2);

 // Temperature Calculation

 adcTemp = (3300 * adcValTemp) / 4096;

 Temp = (adcTemp - 2636) / -13.6;

   //itoa(adcValTemp, string_adcValTemp, 10);

   //CDC_Transmit_FS(string_adcValTemp, strlen((const char*)string_adcValTemp));

 CDC_Transmit_FS(adcValTemp, sizeof(adcValTemp));

}

  HAL_Delay(500);

if (HAL_ADC_PollForConversion(&hadc1, 10) == HAL_OK)

{

 adcVal = HAL_ADC_GetValue(&hadc1);

   itoa(adcVal, string_adcVal, 10);

   CDC_Transmit_FS(string_adcVal, strlen((const char*)string_adcVal));

}

  HAL_Delay(500);

 }

4 REPLIES 4
MSchmutz
Associate II

here i also go the c# code

  public partial class Form1 : Form

  {

    string inbuffer;

    public Form1()

    {

      InitializeComponent();

      serialPort1.Open();

    }

    private void DisplayText(object sender, EventArgs e)

    {

      label1.Text = Convert.ToString(inbuffer);

    }

    private void serialPort1_DataReceived(object sender, System.IO.Ports.SerialDataReceivedEventArgs e)

    {

      inbuffer = serialPort1.ReadExisting();

      this.Invoke(new EventHandler(DisplayText));

    }

  }

}

TDK
Guru

Read both values and send them at the same time within the same USB packet. In your reception program, you will need to unpack them again in the proper order.

If you feel a post has answered your question, please click "Accept as Solution".

could you do me a little example ? i dont get it thanks :D

MM..1
Chief II

In your code you mix value types ... binary data send ... ascii data send

adcValTemp = HAL_ADC_GetValue(&hadc2);
...
CDC_Transmit_FS(adcValTemp, sizeof(adcValTemp));

Too you say how can i read two adc at the same time,

but used code differ. For same moment measure you need triggered ADC not polled, and wait read result in IT or DMA mode....