‎2020-05-30 05:30 PM
When generate the project for the CM4 core, it seems I forget to enabled the SWD debug. Now, in Keil's debug wizard, the SWDIO shows 'No target connected'. My nucleo board is just a brick now.
​
Any method to unlock it?
BTW: I can reboot with BOOT0 pull high, it can recognize the board, and then I can download code for CM7, but not CM4. For CM4, it shows "Internal parameter error"...................
Many many Thanksssssssssssssssssssssss
‎2021-05-27 01:09 PM
Did you ever sort this out? I am seeing it too.
‎2021-06-02 07:00 AM
No, I didn't find a solution to this problem, the board is dead for me now. Hope you can figure out. 😂