cancel
Showing results for 
Search instead for 
Did you mean: 

HELP !! FMC what is going on

JHERI
Senior

Hello

any help appreciated

trying to work out out how the FMC peripheral works on the STM32F767ZI arm

would like to interface an FPGA to the 767 arm as an external memory device using a multiplexed Address & Data Bus, but so little info on the FMC out there ???

I have hooked up all the hardware wiring between the FPGA and ARM and guess what, as usual really really strange thing happening ?

why when I use

 HAL_SRAM_Read_16b(&hsram1, (uint32_t *)0x60000001, (uint16_t *)rxBuffer, 1);

I get two chip selects and two reads

Yet when I read 60000000 I only get one CS and one read, WHAT IS GOING ON ???

 HAL_SRAM_Read_16b(&hsram1, (uint32_t *)0x60000000, (uint16_t *)rxBuffer, 1);

Both these above HAL_SRAM_Read commands should simply read back ONE 16bit (2byte) data from the selected address

but anything above 0x60000000 does 2 chip selects and two reads of the data

is this a floored faulty FMC module

0x60000000 should = 1st 16bit address read

and

0x60000001 should - 2nd 16 bit address read (why 2 chip selects and 2 reads of data ??)

any help appreciated

Thank You

0690X00000Arrz3QAB.jpg

0690X00000Arrz8QAB.jpg

0690X00000ArryoQAB.jpg

0690X00000ArrzDQAR.jpg

0690X00000ArrzNQAR.jpg

9 REPLIES 9

How wide is the DATA BUS?

At 16-bit the memory address to the DEVICE changes from 0x60000000 to 0x60000002

If you read a 16-bit word at an ODD boundary it spans TWO words in the DEVICE

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JHERI
Senior

hello

thank you for your reply

my data bus is 16 bits wide, i'm only interested in 16 bits address so address (16:23) not intrested

so I have 16 multiplexed address and data lines which should hopefully send out the 16bit address first over the 16 lines to the FPGA and then either write or read 16bits of data from or to the FPGA

so am I correct in thinking

0x60000000 = address 0 inside my FPGA

and 0x60000001 = address 1 inside my FPGA

and 0x60000002 = address 2 inside my FPGA

sorry I don't really understand ???

How wide is the DATA BUS? 16bits

At 16-bit the memory address to the DEVICE changes from 0x60000000 to 0x60000002

If you read a 16-bit word at an ODD boundary it spans TWO words in the DEVICE

How can I get over this ???

I simply would like to read or write only 16bits, not two lots of 8bits

Just a simple 16bit read or write of data

Thanks for any help

 would I be better using a different CS memory address area for 16bit read and write say CS3 0x6800000 ???

sorry really confused are you saying it reads two lots of 8bit data consecutively thus the two cs lows ??

is there no way just to simply read and write 16bits of data

thanks

>>so am I correct in thinking

 0x60000000 = address 0 inside my FPGA

 and 0x60000001 = address 1 inside my FPGA

 and 0x60000002 = address 2 inside my FPGA

NO

With a 16-bit DATA BUS the DEVICE addresses as WORDS

 0x60000000 = address 0 externally

 and 0x60000002 = address 1

 and 0x60000004 = address 2

>>sorry really confused are you saying it reads two lots of 8bit data consecutively thus the two cs lows ??

EVEN WORDs will go to your device directly

ODD ADDRESSED WORDs will span TWO WORDs in your DEVICE

0x60000001 will pull HALF of WORD 0, and HALF of WORD 1

BYTEs are manage via BYTE LANES. A Barrel shifter on the input to extract a 8-bit byte from the word, and a LOW/HIGH Byte Lane select for writes to a single byte within the word.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

ST Shifts the Internal Address Space to the External Bus, at 16-bit, ie IntA1 -> ExtA0

0690X00000Ars1xQAB.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JHERI
Senior

thank you very much for your detailed info

so if i'm understanding you correctly

for me to read or write 16bits of data to the FPGA with a single chip correctly , I simply need to issue even address, 0x6000000, 0x60000002, 0x60000004 etc

if I issue odd address, I read or write half the data from one address and half from the next address ???

is this correct

really appreciate your help, as this has really confused me for the past day or so

Regards

YES

The processor has byte addressability, you're attaching a word addressable device, there is a translation

For uint16_t *p = ( uint16_t *)0x60000000;

*p++ = 0x1234; // Writes to DEVICE ADDR 0

*p++ = 0x5678; // Writes to DEVICE ADDR 1 (advances pointer by 2)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JHERI
Senior

Thank you so much :-)

JHERI
Senior

Hello again

so I guess I can not easily read consecutive data in a buffer array say 8bytes starting at 0x60000000

HAL_SRAM_Read_16b(&hsram1, (uint32_t *)0x60000000, (uint16_t *)rxBuffer, 8 );

or can I just ignore the odd data bytes in the array :-)

Regards

turboscrew
Senior III

If your chip can handle unaligned data (I guess most STM32s can), you can read 16-bit data from an odd address. The HW just splits the access into 2 byte accesses, but the value should be right in the destination register. You can also read array of half words starting from zero, or array of bytes starting from zero. What's the problem here?