2022-04-12 3:54 AM
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t read_opcode ;
uint8_t read_addr ;
uint8_t Result_read = 0x00;
uint8_t Result_read_buff=0x00;
char*commande;
commande = (unsigned char *) 0x5A;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SPI1_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4, GPIO_PIN_SET);
HAL_Delay(10);
//Read Data
//1.PUT CS LOW
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
//2.Transmit Register Adresse!
HAL_SPI_Transmit(&hspi1,&read_opcode,1,100);
HAL_SPI_Transmit(&hspi1,&read_addr,1,100);
//3.Read
HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100);
Result_read |= (Result_read_buff);
return Result_read;
//Bring CS High-Desactivation
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
//UART_Communication
commande ="RC_RAA_RD";
HAL_UART_Receive(&huart2,commande,10,1700);
HAL_UART_Transmit(&huart2,&Result_read, 8, 1700);
2022-04-12 4:57 AM
> return Result_read;
Never return from main. It's unclear why this statement is in there.
> char*commande;
> commande = (unsigned char *) 0x5A;
> HAL_UART_Receive(&huart2,commande,10,1700);
You're writing 10 bytes to address 0x5A here, which is unlikely what you want. Define it as an array of length 10+ if you want to receive 10 bytes of data.
> uint8_t Result_read = 0x00;
> HAL_UART_Transmit(&huart2,&Result_read, 8, 1700);
Sending 8 bytes when the variable is only 1 long doesn't make any sense.
These are basic C concepts. I would recommend brushing up on C pointers in general, or following existing SPI/UART example code.
2022-04-12 3:49 PM
There is no point in trying to "develop" firmware for MCU without understanding the basics of C programming. Start with this on a PC: