2019-09-25 11:37 PM
Use STM32F405's SPI + DMA as a slave, circular mode, DMA 16bytes interrupt, but every time send 16bytes to master, the first byte is always the byte that last frame's last byte , it looks like spi tx register is not clear, always contain the last byte, so my question is how can i avoid this problem?
2019-09-26 2:42 AM
The slave sends the same byte two times, once at the end of the previous frame and then again at the beginning of the next frame?
Is there some NSS activity from the master?
Post relevant oscilloscope/logic analyzer screenshots.
JW
2019-09-26 3:40 AM
Reset always the SPI after communication ended, for debug.
2019-09-26 6:58 PM
hi,
No NSS activity from master, just three lines, slave send(hex) A5 06 00 40 00 02 0B BB 0B 00 AA AA AA AA AA AA
but master receive (hex) AA A5 06 00 40 00 02 0B BB 0B 00 AA AA AA AA AA everytime, looks like last AA is always in the spi tx register
2019-09-26 6:59 PM
hello. what function do i use to reset spi communication?
is this the only way?
2019-09-26 10:23 PM
it should be somewhere in RCC or SYS of reference manual. Sorry, don't have time to browse and pinpoint anymore.
The reset will work across all the SPI generations. Other milder fix won't cross generation IP boundaries (especially the one with 32 bit FIFOs)
2019-09-26 10:51 PM
Thanks, i find this function “__HAL_RCC_SPI1_FORCE_RESET()�?,but if i reset spi by using this, do i have to initialize SPI again ?
2019-09-26 11:11 PM
Then this is classical mis-synchronization, the master starts somewhat sooner than the slave, so when master starts clocking slave has not prepared data yet, and master sees some bogus data as the very first byte (maybe 0xFF or 0x00, depends on circumstances).
You need to concentrate on the very beginning of the communication just after reset, probably you'll need to signal somehow from slave to master that slave is ready.
JW
2019-09-26 11:35 PM
hi JW
actually, i'm sure slave is ready, because when i see the slave spi tx buffer is already loaded with new data then i start next master transmit manually, but the first byte is still 0xAA when master received, i think 0xAA is the last byte that last frame send , it stays in spi tx register, am i right?
2019-09-27 1:52 AM
The DMA stores a byte into the SPI Tx holding register whenever it sees it is empty.
So yes, 0xAA is from the end of the previous transaction.
I meant, if you control the very first transaction after reset, you shouldn't run into this kind of mis-synchronization. If the slave has always exactly16 bytes to transfer, and the master will always receive 16 bytes, ever since from the reset, you can't see the pattern you see.
JW