2021-02-22 1:42 AM
Hello,
I've been trying to transfer some data from AXI-SRAM to DTCM via MDMA but it seems not functional.
The transfer occurs the flag of end of transfer is set yet the data that I have in my DTCM isn't the orignal one contained in the AXI-SRAM.
Also important point to note is that I don't have an error flag.
I have reduced everything to a minimum but yet it doesn't seems functional.
Here is some bits of my code:
#define ADC_IN_BUFFER_SIZE 10
__attribute__ ((section(".axi"), used)) uint16_t RandomBuffer[ADC_IN_BUFFER_SIZE]={0x0000};
__attribute__ ((section(".dtcm"), used)) uint16_t samplingBuffer[ADC_IN_BUFFER_SIZE]={0x0000};
void MX_MDMA_Init(void)
{
//switching on the clock for MDMA
LL_AHB3_GRP1_EnableClock(LL_AHB3_GRP1_PERIPH_MDMA);
NVIC_SetPriority(MDMA_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(MDMA_IRQn);
LL_MDMA_SetTriggerMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BLOCK_TRANSFER);
LL_MDMA_SetRequestMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_REQUEST_MODE_SW);
LL_MDMA_SetDestinationDataSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_DATA_SIZE_HALFWORD);
LL_MDMA_SetSourceDataSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_DATA_SIZE_HALFWORD);
LL_MDMA_SetDestinationIncMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_INCREMENT);
LL_MDMA_SetSourceIncMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_INCREMENT);
LL_MDMA_SetDestinationIncSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_INC_OFFSET_HALFWORD);
LL_MDMA_SetSourceIncSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_INC_OFFSET_HALFWORD);
LL_MDMA_SetBufferTransferLength(MDMA, LL_MDMA_CHANNEL_0, 1);
LL_MDMA_SetChannelPriorityLevel(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_PRIORITY_VERYHIGH);
LL_MDMA_SetDestinationAddress(MDMA, LL_MDMA_CHANNEL_0, (uint32_t) samplingBuffer);
LL_MDMA_SetSourceAddress(MDMA, LL_MDMA_CHANNEL_0, (uint32_t) RandomBuffer);
LL_MDMA_SetDestBusSelection(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_BUS_AHB_TCM);
LL_MDMA_SetSrcBusSelection(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_BUS_SYSTEM_AXI);
LL_MDMA_SetBlkRepeatCount(MDMA, LL_MDMA_CHANNEL_0, 0);
LL_MDMA_SetBlkRepeatDestAddrUpdate(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BLK_RPT_DEST_ADDR_DECREMENT);
LL_MDMA_SetBlkRepeatSrcAddrUpdate(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BLK_RPT_SRC_ADDR_DECREMENT);
LL_MDMA_SetBlkRptDestAddrUpdateValue(MDMA, LL_MDMA_CHANNEL_0,ADC_IN_BUFFER_SIZE);
LL_MDMA_SetBlkRptSrcAddrUpdateValue(MDMA, LL_MDMA_CHANNEL_0,ADC_IN_BUFFER_SIZE);
LL_MDMA_EnableIT_BT(MDMA, LL_MDMA_CHANNEL_0);
LL_MDMA_EnableIT_TE(MDMA, LL_MDMA_CHANNEL_0);
LL_MDMA_EnableIT_TC(MDMA, LL_MDMA_CHANNEL_0);
}
void MDMA_Start(void)
{
LL_MDMA_SetBlkDataLength(MDMA, LL_MDMA_CHANNEL_0, ADC_IN_BUFFER_SIZE);
LL_MDMA_EnableChannel(MDMA, LL_MDMA_CHANNEL_0);
}I call the MX_MDMA_Init() function along with others standard inits and the MDMA_Start() just before the software triggering.
Any clues why things aren't working as intended?
Seb
Solved! Go to Solution.
2021-02-22 2:48 AM
Okay,
Apparently it is my bad.
It seems that if DCache is used meanwhile MDMA transfers data the transfer gets strange and full of irrelevant data.
Seb
2021-02-22 2:48 AM
Okay,
Apparently it is my bad.
It seems that if DCache is used meanwhile MDMA transfers data the transfer gets strange and full of irrelevant data.
Seb