2024-11-07 6:46 AM
I want to drive havfbridge with STM32G474. I am going to use TIMx with channel1 and channel2 to create two PWM signals, that are 180° out of phase and with the same PWM % that is limited to 0% < PWM % < 49%. Because tohose signals have max 50% duty cycle and are 180° out of phase, they cant be bot high at once.
I already have code with multiple __HAL_TIM_SET_COMPARE calls, but i heard about Complementary outputs.
I dont find settings for this in my Cube MX , can anyone help? Does STM32G474 have that or only STM32F series?
Here are manuals:
https://www.st.com/resource/en/reference_manual/rm0440-stm32g4-series-advanced-armbased-32bit-mcus-stmicroelectronics.pdf
And pages:
28.3.17 for timers TIM1, TIM8 and TIM20
and
30.4.14 for timers TIM15, TIM16 and TIM17
2025-01-08 3:02 AM
Hello @Miha,
Yes, the STM32G474 does support complementary PWM outputs.
You can refer to the example provided in the STM32G4 Cube package: STM32CubeG4/Projects/NUCLEO-G474RE/Examples/TIM/TIM_ComplementarySignals at master · STMicroelectronics/STM32CubeG4
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.