2023-03-08 5:35 AM
Hello,
I tried the Hal_Delay function but it's not work Do you have any idea for this error ?
And my code still waits at this loop :
Thank you for your helps
Regards
2023-12-05 2:07 PM
LCE,
I added this code that flashes an LED between purple and green at 100ms intervals but the code locks at the first call to Hal_Delay(). If I comment out the first while loop so that my delay function is used instead, the LEDs flash as expected so I know the interrupts are enabled (my functions use them):
HAL_InitTick(0); // TICK_INT_PRIORITY = 0
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SysTick_IRQn);
while(1)
{
HAL_Delay(100);
ledOverride(IC_PUR);
HAL_Delay(100);
ledOverride(IC_GRN);
}
while(1)
{
timerDelay(100);
ledOverride(IC_PUR);
timerDelay(100);
ledOverride(IC_GRN);
}
2023-12-05 2:09 PM
Thank you DYann.1. I do have the Timebase Source set to SysTick.
2023-12-05 2:19 PM
Karl,
I have attached my .ioc file.
Thank you looking at it.
Interesting, I tried to attach my .ioc file and won't allow me to stating that it's contents do not match the .ioc extension. However, I just dragged it from my project folder. I tried to .zip but it won't allow .zip files either. Is it possible that my file is corrupt?
2023-12-05 2:24 PM
It won't let me attach the .ioc file.
2023-12-05 2:28 PM
2023-12-05 2:39 PM
Is it possible that my file is corrupt?
The megacompany owned parodies of forums are developed and managed by people, who do not use or understand what a forum is.
https://community.st.com/t5/feedback-forum/please-support-zip-attachments/td-p/580074
2023-12-05 3:12 PM
I hope I didn't do anything wrong. I was able to send the .ioc file in .7z format. I should have read what types of files it would accept first...