2024-03-17 4:42 PM
Hi
I am using CAN in STM32F303RDT6.
I am using HAL_CAN_AddTxMessage for CAN transmission.
This function will send the data and return HAL_OK if the sending mailbox is free.
However, although HAL_CAN_AddTxMessage returns HAL_OK, no message may actually be output on the CAN bus.
I am using CANoe to monitor a CAN bus.
My application has a queue that stores outgoing messages that I create. The application writes outgoing data to the queue at any time.
The data retrieved from the queue is input to HAL_CAN_AddTxMessage. When HAL_OK is returned, it is assumed that the data has been sent and the next queue data is retrieved.
However, even though HAL_OK is returned, there are times when it is not output to the CAN bus. This is a problem.
Please tell me any countermeasures.
Help Me.....
Solved! Go to Solution.
2024-03-17 7:51 PM
Hi
The problem was resolved by setting bit 4 of the CAN_MCR register to 0.
I think that if you are using CAN, the initial value of bit4 should be "0".
2024-03-17 7:51 PM
Hi
The problem was resolved by setting bit 4 of the CAN_MCR register to 0.
I think that if you are using CAN, the initial value of bit4 should be "0".
2024-12-23 4:55 AM
Hi UKAZU
I need your help same I am trying to send two different CAN ID ,.
Can you help me ?
B.R
Ashish