2023-09-01 02:55 AM
When I try to use X-CUBE-FREERTOS on H573 board, there is a warning sign and it is impossible to install.
How do I install X-CUBE-FREERTOS bundle for CubeMX?
Thanks!
Solved! Go to Solution.
2023-09-01 03:47 AM
Hello @Artomatica and welcome to the Community 🙂
You should first install the X-Cube-FREERTOS package from: Help > Manage embedded software packages > STMicroelectronics.
Imen
2023-09-01 03:47 AM
Hello @Artomatica and welcome to the Community 🙂
You should first install the X-Cube-FREERTOS package from: Help > Manage embedded software packages > STMicroelectronics.
Imen
2023-09-07 04:07 AM
Thanks, login into the account fixed the problem.