2025-01-11 04:35 AM - last edited on 2025-01-11 06:05 AM by Andrew Neil
I want to use led with following connection and i remember that I've seen this application somewhere on the Internet:
3V3 - LED - RESISTOR - STM32 PIN
I've seen the max total current output of MCU then is there any max total input current of MCU?
Solved! Go to Solution.
2025-01-11 05:38 AM - edited 2025-01-11 05:38 AM
2025-01-11 05:38 AM - edited 2025-01-11 05:38 AM
2025-01-11 05:43 AM
does "injected current" mean input current?
2025-01-11 05:48 AM
I don't think so - context needed.
You are looking for the GPIO pin current sink capacity.
What chip are you using?
2025-01-11 05:49 AM
I currently use STM32H750VBT6
2025-01-11 05:55 AM
I think I found the answer... maximum is 8mA w constant Voh and Vol and maximum 20mA with relaxed Voh and Vol...
2025-01-11 06:02 AM
That's for one pin.
If you've got lots of LEDs, beware that there's also a maximum total for the whole chip ...
2025-01-11 06:03 AM
Thank you so much!