2016-04-13 02:25 PM
Hi,
I facing problem with custom segment glass LCD interfacing which include 4 COM pin and 20 SEGMENT pin with 1/4 duty cycle and 1/3 bias (Refer Attachment).I tries to understanding HAL library provided on ST site example project but, I can't understand the RAM part.Please suggest me, is more information/documents require to interface Glass LCD ? Please help me.thank you. #glass-lcd #stm32l02018-08-24 09:47 PM
Do you find any solution regarding this custom glass.\
If yes Than please share me the some solution so that i also can drive it.