General Purpose Timers: what are the options for One-Pulse slave mode trigger?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-03 7:10 PM
I am using STM32H7 General Purpose Timers TIM2, TIM3, TIM4, TIM5 and their respective external trigger ETR using combined RESET and TRIGGER modes and I am configuring and starting Channel4 for each to generate One-Pulse output .
All the configuration and startup steps followed, Base counter started, Channels started but It does not work.
All the One-Pulse examples I found in STM app notes and on-line examples show only one case of the Timer slave mode for One-Pulse generation: using the TI1FP1 or TI2FP2 inputs from the channel pins. Not ETR, not ITx examples , but only those two.
I suspect that only these inputs triggers are allowed for the Timer One-Pulse mode but the user manual on One-Pulse Ch. 39.3.13 fails to mention that.
User guide for STM32H7 One-pulse mode Ch. 39.3.13 states:
Starting the counter can be controlled through the slave mode controller.
No limitations have been mentioned regarding the trigger choice for the Timer slave mode , although Chapters on General Purpose timers describe different types of possible external and internal triggers, including external trigger ETR
So the question is: can ETR trigger be used to reset and trigger the internally clocked timer counter and generate One-Pulse channel output?
Solved! Go to Solution.
- Labels:
-
STM32H7 Series
-
TIM
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-14 6:10 PM
I came back to provide the answer to my question for those who may have the same problem.
The chip indeed allows One-pulse generation while triggering the slave with any of the possible slave triggers: ETR, internal triggers ITx, or input channels TI1FP1 or TI1FP2. But using HAL libraries generated by CubeMX will fail for any triggers except TI1FP1 and TI1FP2.
The HAL libraries for One-pulse generated by CubeMX written in such way that the function calls expect only two channels 1 and 2 used TI1FP1 and TI1FP2 as a trigger.
The team who wrote that code was so much convinced that this is the only allowed slave trigger for one-pulse that even STM App note dedicated to the One-pulse generation (I read it long ago and lost that link now) says that user "has to configure" TI1FP1 and TI1FP2 as a trigger following the steps. Text does not allow any other alternatives. All docs from STM32 insist on only these two triggers.
Once I replace HAL functions with my code directly controlling the MCU registers following only the MCU datasheet, my ETR trigger successfully triggered One-pulse .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-03 11:12 PM
Read out and check/post content of TIM and relevant GPIO registers for one of the timers.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-14 6:10 PM
I came back to provide the answer to my question for those who may have the same problem.
The chip indeed allows One-pulse generation while triggering the slave with any of the possible slave triggers: ETR, internal triggers ITx, or input channels TI1FP1 or TI1FP2. But using HAL libraries generated by CubeMX will fail for any triggers except TI1FP1 and TI1FP2.
The HAL libraries for One-pulse generated by CubeMX written in such way that the function calls expect only two channels 1 and 2 used TI1FP1 and TI1FP2 as a trigger.
The team who wrote that code was so much convinced that this is the only allowed slave trigger for one-pulse that even STM App note dedicated to the One-pulse generation (I read it long ago and lost that link now) says that user "has to configure" TI1FP1 and TI1FP2 as a trigger following the steps. Text does not allow any other alternatives. All docs from STM32 insist on only these two triggers.
Once I replace HAL functions with my code directly controlling the MCU registers following only the MCU datasheet, my ETR trigger successfully triggered One-pulse .