2025-01-24 05:33 PM
Hi,
I have interfaced an STM32H723 to an MRAM that is SRAM compatible, using FMC.. The memory is SRAM compatible, 20bit address and 16bit data. The main control pins for the memory are: CHIP ENABLE (~E), WRITE ENABLE (~W) and OUTPUT ENABLE (~G). FMC clock is 64MHz. System clock is 64MHz.
The problem(s):
1. in my example, HAL_SRAM_Read_16b works correctly. ~E and ~G are triggered, and data is read correctly.
2. in my example, HAL_SRAM_Write_16b does not trigger either ~E, nor ~W. Writing happens (can see it in Memory View in STM32CubeIde) but it is not actually saved in the MRAM. Therefore, data is lost in the next reset of the uC.
3. Surprisingly, if I open a Memory View in STM32CubeIde and write in memory "by hand", ~E and ~W get triggered (correct functionality!).
All examples give HAL_OK as result. I have two questions regarding this:
Thank you so much in advance.
More information:
FMC config:
MPU config:
Code (main.c):
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define BUFFER_SIZE ((uint32_t)0x0010)
#define WRITE_READ_ADDR ((uint32_t)0x0900)
#define SRAM_BANK_ADDR ((uint32_t)0x60000000)
/* #define SRAM_MEMORY_WIDTH FMC_NORSRAM_MEM_BUS_WIDTH_8 */
#define SRAM_MEMORY_WIDTH FMC_NORSRAM_MEM_BUS_WIDTH_16
#define SRAM_TIMEOUT ((uint32_t)0xFFFF)
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
SRAM_HandleTypeDef hsram1;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_FMC_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* Read/Write Buffers */
//uint32_t aTxBuffer[BUFFER_SIZE];
//uint32_t aRxBuffer[BUFFER_SIZE];
/* Status variables */
__IO uint32_t writeReadStatus = 0;
/* Counter index */
uint32_t uwIndex = 0;
uint32_t compare_uint16_buffers(const uint16_t *buffer1, const uint16_t *buffer2, uint16_t bufSize) {
for (int i = 0; i < bufSize; i++) {
if (buffer1[i] != buffer2[i]) {
return 0; // Buffers differ at index i
}
}
return 1; // Buffers are identical
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FMC_Init();
/* USER CODE BEGIN 2 */
/* ######## SRAM memory read/write access ######################################*/
uint16_t sram_aTxBuffer[BUFFER_SIZE] = {0x00, 0x01, 0x02, 0x03,
0x04, 0x05, 0x06, 0x07,
0x08, 0x09, 0x0A, 0x0B,
0x0C, 0x0D, 0x0E, 0x0F};
uint16_t sram_aRxBufferInitial[BUFFER_SIZE]= {0};
uint16_t sram_aRxBufferFinal[BUFFER_SIZE]= {0};
HAL_StatusTypeDef resRxInitial = HAL_SRAM_Read_16b(&hsram1, (uint32_t *)(SRAM_BANK_ADDR + WRITE_READ_ADDR), (uint16_t *)sram_aRxBufferInitial, BUFFER_SIZE);
/* Write data to the SRAM memory */
HAL_StatusTypeDef resTx = HAL_SRAM_Write_16b(&hsram1, (uint32_t *)(SRAM_BANK_ADDR + WRITE_READ_ADDR), (uint16_t *)sram_aTxBuffer, BUFFER_SIZE);
/* Read back data from the SRAM memory */
HAL_StatusTypeDef resRxFinal = HAL_SRAM_Read_16b(&hsram1, (uint32_t *)(SRAM_BANK_ADDR + WRITE_READ_ADDR), (uint16_t *)sram_aRxBufferFinal, BUFFER_SIZE);
/* ######## Checking data integrity ############################################*/
writeReadStatus = compare_uint16_buffers(sram_aTxBuffer, sram_aRxBufferInitial, BUFFER_SIZE);
if(writeReadStatus) {
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
/* FMC initialization function */
static void MX_FMC_Init(void)
{
/* USER CODE BEGIN FMC_Init 0 */
/* USER CODE END FMC_Init 0 */
FMC_NORSRAM_TimingTypeDef Timing = {0};
/* USER CODE BEGIN FMC_Init 1 */
/* USER CODE END FMC_Init 1 */
/** Perform the SRAM1 memory initialization sequence
*/
hsram1.Instance = FMC_NORSRAM_DEVICE;
hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
/* hsram1.Init */
hsram1.Init.NSBank = FMC_NORSRAM_BANK1;
hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
hsram1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
/* Timing */
Timing.AddressSetupTime = 3;
Timing.AddressHoldTime = 15;
Timing.DataSetupTime = 3;
Timing.BusTurnAroundDuration = 1;
Timing.CLKDivision = 16;
Timing.DataLatency = 17;
Timing.AccessMode = FMC_ACCESS_MODE_A;
/* ExtTiming */
if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
{
Error_Handler( );
}
/* USER CODE BEGIN FMC_Init 2 */
/* USER CODE END FMC_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/* MPU Configuration */
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x60000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_2MB;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Code: stm32h7xx_hal_msp.c
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file stm32h7xx_hal_msp.c
* @brief This file provides code for the MSP Initialization
* and de-Initialization codes.
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */
/* USER CODE END TD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN Define */
/* USER CODE END Define */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN Macro */
/* USER CODE END Macro */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* External functions --------------------------------------------------------*/
/* USER CODE BEGIN ExternalFunctions */
/* USER CODE END ExternalFunctions */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* Initializes the Global MSP.
*/
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_SYSCFG_CLK_ENABLE();
/* System interrupt init*/
/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}
static uint32_t FMC_Initialized = 0;
static void HAL_FMC_MspInit(void){
/* USER CODE BEGIN FMC_MspInit 0 */
/* USER CODE END FMC_MspInit 0 */
GPIO_InitTypeDef GPIO_InitStruct ={0};
if (FMC_Initialized) {
return;
}
FMC_Initialized = 1;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FMC;
PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_D1HCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_FMC_CLK_ENABLE();
/** FMC GPIO Configuration
PE3 ------> FMC_A19
PF0 ------> FMC_A0
PF1 ------> FMC_A1
PF2 ------> FMC_A2
PF3 ------> FMC_A3
PF4 ------> FMC_A4
PF5 ------> FMC_A5
PC0 ------> FMC_D12
PA4 ------> FMC_D8
PA5 ------> FMC_D9
PF12 ------> FMC_A6
PF13 ------> FMC_A7
PF14 ------> FMC_A8
PF15 ------> FMC_A9
PG0 ------> FMC_A10
PG1 ------> FMC_A11
PE7 ------> FMC_D4
PE8 ------> FMC_D5
PE9 ------> FMC_D6
PE10 ------> FMC_D7
PE13 ------> FMC_D10
PE14 ------> FMC_D11
PD8 ------> FMC_D13
PD9 ------> FMC_D14
PD10 ------> FMC_D15
PD11 ------> FMC_A16
PD12 ------> FMC_A17
PD13 ------> FMC_A18
PD14 ------> FMC_D0
PD15 ------> FMC_D1
PG2 ------> FMC_A12
PG3 ------> FMC_A13
PG4 ------> FMC_A14
PG5 ------> FMC_A15
PC7 ------> FMC_NE1
PD0 ------> FMC_D2
PD1 ------> FMC_D3
PD4 ------> FMC_NOE
PD5 ------> FMC_NWE
PE0 ------> FMC_NBL0
PE1 ------> FMC_NBL1
*/
GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9
|GPIO_PIN_10|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_0
|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_12|GPIO_PIN_13
|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF1_FMC;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
|GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11
|GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15
|GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF9_FMC;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USER CODE BEGIN FMC_MspInit 1 */
/* USER CODE END FMC_MspInit 1 */
}
void HAL_SRAM_MspInit(SRAM_HandleTypeDef* hsram){
/* USER CODE BEGIN SRAM_MspInit 0 */
/* USER CODE END SRAM_MspInit 0 */
HAL_FMC_MspInit();
/* USER CODE BEGIN SRAM_MspInit 1 */
/* USER CODE END SRAM_MspInit 1 */
}
static uint32_t FMC_DeInitialized = 0;
static void HAL_FMC_MspDeInit(void){
/* USER CODE BEGIN FMC_MspDeInit 0 */
/* USER CODE END FMC_MspDeInit 0 */
if (FMC_DeInitialized) {
return;
}
FMC_DeInitialized = 1;
/* Peripheral clock enable */
__HAL_RCC_FMC_CLK_DISABLE();
/** FMC GPIO Configuration
PE3 ------> FMC_A19
PF0 ------> FMC_A0
PF1 ------> FMC_A1
PF2 ------> FMC_A2
PF3 ------> FMC_A3
PF4 ------> FMC_A4
PF5 ------> FMC_A5
PC0 ------> FMC_D12
PA4 ------> FMC_D8
PA5 ------> FMC_D9
PF12 ------> FMC_A6
PF13 ------> FMC_A7
PF14 ------> FMC_A8
PF15 ------> FMC_A9
PG0 ------> FMC_A10
PG1 ------> FMC_A11
PE7 ------> FMC_D4
PE8 ------> FMC_D5
PE9 ------> FMC_D6
PE10 ------> FMC_D7
PE13 ------> FMC_D10
PE14 ------> FMC_D11
PD8 ------> FMC_D13
PD9 ------> FMC_D14
PD10 ------> FMC_D15
PD11 ------> FMC_A16
PD12 ------> FMC_A17
PD13 ------> FMC_A18
PD14 ------> FMC_D0
PD15 ------> FMC_D1
PG2 ------> FMC_A12
PG3 ------> FMC_A13
PG4 ------> FMC_A14
PG5 ------> FMC_A15
PC7 ------> FMC_NE1
PD0 ------> FMC_D2
PD1 ------> FMC_D3
PD4 ------> FMC_NOE
PD5 ------> FMC_NWE
PE0 ------> FMC_NBL0
PE1 ------> FMC_NBL1
*/
HAL_GPIO_DeInit(GPIOE, GPIO_PIN_3|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9
|GPIO_PIN_10|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_0
|GPIO_PIN_1);
HAL_GPIO_DeInit(GPIOF, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_12|GPIO_PIN_13
|GPIO_PIN_14|GPIO_PIN_15);
HAL_GPIO_DeInit(GPIOC, GPIO_PIN_0|GPIO_PIN_7);
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_4|GPIO_PIN_5);
HAL_GPIO_DeInit(GPIOG, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
|GPIO_PIN_4|GPIO_PIN_5);
HAL_GPIO_DeInit(GPIOD, GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11
|GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15
|GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5);
/* USER CODE BEGIN FMC_MspDeInit 1 */
/* USER CODE END FMC_MspDeInit 1 */
}
void HAL_SRAM_MspDeInit(SRAM_HandleTypeDef* hsram){
/* USER CODE BEGIN SRAM_MspDeInit 0 */
/* USER CODE END SRAM_MspDeInit 0 */
HAL_FMC_MspDeInit();
/* USER CODE BEGIN SRAM_MspDeInit 1 */
/* USER CODE END SRAM_MspDeInit 1 */
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
Solved! Go to Solution.
2025-01-28 12:13 PM
Hello,
For this kind of issue/behavior, start by disabling the cache either by using MPU or just do not enable it at your program start.
2025-01-28 12:13 PM
Hello,
For this kind of issue/behavior, start by disabling the cache either by using MPU or just do not enable it at your program start.
2025-01-28 02:58 PM
Thank you very much @SofLit . Removing those two lines solved the problem:
/* Enable I-Cache---------------------------------------------------------*/
//SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
//SCB_EnableDCache();
A question remains: Why does this affect the FMC and prevents the activation of the data writing?