2024-12-20 01:48 AM - last edited on 2024-12-20 02:03 AM by Andrew Neil
Hello,
We are migrating to zephyr, the board which is supported by zephyr is nucleo_g0b1re, but out actual controller is stm32g0c1ret3. Both are of same family, have same memory and all. I have just made changes in the overlay file for my application, have not touched anything in .dtsi or .dts file. I am facing issue when i try to dump code my my led which i have added in the overlay file. The error says "[stm32g0x.cpu] halted due to breakpoint, current mode: Handler HardFault". Can anyone tell what the possible ways can be due to which this error is occurring while flashing.
I have attached the screenshot of error.
2024-12-20 02:03 AM
What development host platform?
What tools & versions?
Can you program anything else using this environment? eg, an out-of-the-box example?
Can you program using STM32CubeProgrammer?
Have you tried asking at a Zephyr-specific forum?
@vividhadhengre wrote:I have attached the screenshot of error.
It would be more helpful to post it as text - see: