cancel
Showing results for 
Search instead for 
Did you mean: 

FD_CAN How to reset error counter

Aeroiiv
Associate II

In the FD_CAN register, there is a CEL[7:0]:, REC[6:0]: and TEC[7:0]:,

The CEL register is not being reset on read and goes into the Bus-Off mode.

Do I need to also reset the REC and TEC register?

I am currently using the HAL_GetErrorCounter() function to read the register. 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

You need to reset the FDCAN peripheral to reset REC[6:0] and TEC[7:0].

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

You need to reset the FDCAN peripheral to reset REC[6:0] and TEC[7:0].

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

In order to reset the FDCAN peripheral without power cycling the system;

I am currently calling 

HAL_StatusTypeDef HAL_FDCAN_DeInit(FDCAN_HandleTypeDef *hfdcan)

and the reinitializing using 

static void MX_FDCAN1_Init(void)

 

Are there anything else specific that needs to happen, within the DeInit function it only seems to disable the interrupt line CLEAR_BIT(hfdcan->Instance->ILE, (FDCAN_INTERRUPT_LINE0 | FDCAN_INTERRUPT_LINE1));

Do I also need to deinitlize the clock as well?

Hello,

You need to reset FDCAN peripheral by RCC in HAL_FDCAN_MspDeInit(): 

__HAL_RCC_FDCAN_FORCE_RESET();
__HAL_RCC_FDCAN_RELEASE_RESET();

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Is there a difference between using

__HAL_RCC_FDCAN_FORCE_RESET();
__HAL_RCC_FDCAN_RELEASE_RESET();

and using  __HAL_RCC_FDCAN_CLK_DISABLE();

 

In my version of MspDeInit it uses the rather method instead of the force_reset/release_reset.

void HAL_FDCAN_MspDeInit(FDCAN_HandleTypeDef* hfdcan)
{
if(hfdcan->Instance==FDCAN1)
{
/* USER CODE BEGIN FDCAN1_MspDeInit 0 */

/* USER CODE END FDCAN1_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_FDCAN_CLK_DISABLE();

/**FDCAN1 GPIO Configuration
PB12 ------> FDCAN1_RX
PB13 ------> FDCAN1_TX
*/
HAL_GPIO_DeInit(GPIOB, GPIO_PIN_12|GPIO_PIN_13);

/* USER CODE BEGIN FDCAN1_MspDeInit 1 */

/* USER CODE END FDCAN1_MspDeInit 1 */
}

}

 __HAL_RCC_FDCAN_CLK_DISABLE only de-asserts the clock to the peripheral and as soon as you enable it again  the registers content are kept while you're looking for a reset of the registers which can be done by:

__HAL_RCC_FDCAN_FORCE_RESET();
__HAL_RCC_FDCAN_RELEASE_RESET();

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.