cancel
Showing results for 
Search instead for 
Did you mean: 

Failed attempt on using 2 Timers to Toggle GPIO.

Oahme.1
Associate III

Hello , 
I have initialized two timers , Timer3 and Timer9. Im using Timer9 with 137uS period , setting my gpio pin high , starting Tim3 Interrupt with 54uS period for now .When Tim3 Interrupt occurs I simply reset my gpio pin.My problem is that I should have a high pwm for 54uS and 137uS pwm in reset state.I have thoroughly checked individual timers to just toggle single gpio in 1 single interrupt , both give me a stable 137uS pwm and 54uS pwm . But as i use two different gpio's to set and reset my gpio. I get irregular pwm that has values randomly changing. My pwm will have a constant 137uS low and a variable high pwm state which is Max 122uS for now as I said its just fixed 54uS so I also did not enable autoload preload .This is the first time I'm doing it this way.

My Code :

Timer Setting : 

void MX_TIM3_Init(void)
{

  /* USER CODE BEGIN TIM3_Init 0 */

  /* USER CODE END TIM3_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM3_Init 1 */

  /* USER CODE END TIM3_Init 1 */
  htim3.Instance = TIM3;
  htim3.Init.Prescaler = 0;
  htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim3.Init.Period = 4700;
  htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM3_Init 2 */

  //HAL_TIM_Base_Start_IT(&htim3);
  /* USER CODE END TIM3_Init 2 */

}
/* TIM9 init function */
void MX_TIM9_Init(void)
{

  /* USER CODE BEGIN TIM9_Init 0 */

  /* USER CODE END TIM9_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};

  /* USER CODE BEGIN TIM9_Init 1 */

  /* USER CODE END TIM9_Init 1 */
  htim9.Instance = TIM9;
  htim9.Init.Prescaler = 0;
  htim9.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim9.Init.Period = 11508;
  htim9.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim9.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim9) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim9, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM9_Init 2 */
  HAL_TIM_Base_Start_IT(&htim9);
  /* USER CODE END TIM9_Init 2 */

}

void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{

  if(tim_baseHandle->Instance==TIM3)
  {
  /* USER CODE BEGIN TIM3_MspInit 0 */

  /* USER CODE END TIM3_MspInit 0 */
    /* TIM3 clock enable */
    __HAL_RCC_TIM3_CLK_ENABLE();

    /* TIM3 interrupt Init */
    HAL_NVIC_SetPriority(TIM3_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(TIM3_IRQn);
  /* USER CODE BEGIN TIM3_MspInit 1 */

  /* USER CODE END TIM3_MspInit 1 */
  }
  else if(tim_baseHandle->Instance==TIM9)
  {
  /* USER CODE BEGIN TIM9_MspInit 0 */

  /* USER CODE END TIM9_MspInit 0 */
    /* TIM9 clock enable */
    __HAL_RCC_TIM9_CLK_ENABLE();

    /* TIM9 interrupt Init */
    HAL_NVIC_SetPriority(TIM1_BRK_TIM9_IRQn,0, 0);
    HAL_NVIC_EnableIRQ(TIM1_BRK_TIM9_IRQn);
  /* USER CODE BEGIN TIM9_MspInit 1 */

  /* USER CODE END TIM9_MspInit 1 */
  }
}

void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle)
{

  if(tim_baseHandle->Instance==TIM3)
  {
  /* USER CODE BEGIN TIM3_MspDeInit 0 */

  /* USER CODE END TIM3_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_TIM3_CLK_DISABLE();

    /* TIM3 interrupt Deinit */
    HAL_NVIC_DisableIRQ(TIM3_IRQn);
  /* USER CODE BEGIN TIM3_MspDeInit 1 */

  /* USER CODE END TIM3_MspDeInit 1 */
  }
  else if(tim_baseHandle->Instance==TIM9)
  {
  /* USER CODE BEGIN TIM9_MspDeInit 0 */

  /* USER CODE END TIM9_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_TIM9_CLK_DISABLE();

    /* TIM9 interrupt Deinit */
    HAL_NVIC_DisableIRQ(TIM1_BRK_TIM9_IRQn);
  /* USER CODE BEGIN TIM9_MspDeInit 1 */

  /* USER CODE END TIM9_MspDeInit 1 */
  }
}

 

Interrupt Callback function : 

volatile bool temp = true;
volatile bool Flag = true;

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{

	if(htim->Instance == TIM3)
			{
			if(temp)
				{

					temp= false;
				}
				//HAL_TIM_Base_Start_IT(&htim9);
			//__HAL_TIM_ENABLE_IT(htim, TIM_IT_UPDATE);

			if(Flag)
			{
				HAL_GPIO_WritePin(GPIOA, weld_Pin,GPIO_PIN_RESET);

				Flag = false;
				__NOP();
			}

			}

	if(htim->Instance == TIM9)
			{

			if(temp)
			{

				temp= false;
				//HAL_TIM_Base_Init(&htim3);
				HAL_TIM_Base_Start_IT(&htim3);
			}

			//HAL_GPIO_TogglePin(GPIOA,weld_Pin);
			Flag = true;
			HAL_GPIO_WritePin(GPIOA, weld_Pin,GPIO_PIN_SET);
			__NOP();

			}
}

 

Initially I got overconfident and defined the whole structure program which is much complicated hoping this will definitely work , but unfortunately I had to go back to the basics because I was not getting the desired  Timer results.

I will add 2 photos which depict what I want and what I'm actually getting .

Any Help would be great . @Tesla DeLorean @TDK  ,Can you help in this matter ? 

Thanks.

Actual Picture

PWM Actual.jpeg

 

Original Idea

PWM_Orginal.png

 

 

 

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14

Yes , I Believe thats true but Update interrupt not interrupting in there own dedicated functions ? Weird. Trust me man I'm just trying to go along with HAL using basic libraries to get the job done ,otherwise I absolutely hate it . Will shift to LL Drivers but for now I have to get the job done .

@TDK can you help me with the above reply regarding interrupt ? 

Depending on your channel configuration, CCx callbacks are done in one of the following callbacks:

HAL_TIM_IC_CaptureCallback(htim);
HAL_TIM_OC_DelayElapsedCallback(htim);
HAL_TIM_PWM_PulseFinishedCallback(htim);

You can see the logic used for callbacks within HAL_TIM_IRQHandler.

If you feel a post has answered your question, please click "Accept as Solution".
Oahme.1
Associate III

Thanks, Got it, Lastly regarding the Interrupt Priorities , I've I have 2 Timers , Timers 1 is the highest priority and Timer2 is the second highest priority , that means my Preempt Priority is 0 for Timer 1 and 1 for Timer 2 right ?

Yes. Priority 0 will pre-empt priority 1.

If you feel a post has answered your question, please click "Accept as Solution".
Oahme.1
Associate III

Thanks @TDK