cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Simulink: No STM32 MCU Connected

Khadratov
Associate

Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer, MATLAB Simulink is unable to read it. Any help that can be provided will be appreciated!
I appreciate any help you can provide.

 

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @Khadratov and welcome to the ST Comunity.

For this implementation, I suggest you contact Matlab community that is the responsible of the Matlab/Simulink implementation on the STM32 MCUs.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Evangelist III

The first thing to check is whether the ST-Link is actually visible to your computer:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

 


@Khadratov wrote:

Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer...


So STM32CubeProgrammer can connect & works OK ?

Does MATLAB require that you disconnect the CubeProgrammer first ?

If CubeProgrammer connects OK, but MATLAB can't, then it's a MATLAB issue - as @STTwo-32 said, you need to contact MATLAB in that case.