2024-10-22 09:44 AM
Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer, MATLAB Simulink is unable to read it. Any help that can be provided will be appreciated!
I appreciate any help you can provide.
2024-10-22 10:01 AM
Hello @Khadratov and welcome to the ST Comunity.
For this implementation, I suggest you contact Matlab community that is the responsible of the Matlab/Simulink implementation on the STM32 MCUs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-22 10:14 AM
The first thing to check is whether the ST-Link is actually visible to your computer:
@Khadratov wrote:Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer...
So STM32CubeProgrammer can connect & works OK ?
Does MATLAB require that you disconnect the CubeProgrammer first ?
If CubeProgrammer connects OK, but MATLAB can't, then it's a MATLAB issue - as @STTwo-32 said, you need to contact MATLAB in that case.