cancel
Showing results for 
Search instead for 
Did you mean: 

Error in RM0490 Rev. 4 Section 6.2.6

MorganG
Associate

Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.

Should be the following:

Status bits in the RCC clock control register (RCC_CR) indicate which clock(s) is (are) ready.

Status bits in the RCC clock configuration register (RCC_CFGR) indicate which clock is currently used as a system clock.

1 ACCEPTED SOLUTION

Accepted Solutions
Simon.T
ST Employee

Hello @MorganG ,

 

I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

 

Best regards,

 

Simon

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @MorganG and welcome to the Community,

Thank you for raising this issue.

I will check this and will get back to you soon with update (Internal ticket is submitted ID 193408 - not available outside of ST)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Simon.T
ST Employee

Hello @MorganG ,

 

I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

 

Best regards,

 

Simon