2024-10-10 04:43 AM
Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.
Should be the following:
Status bits in the RCC clock control register (RCC_CR) indicate which clock(s) is (are) ready.
Status bits in the RCC clock configuration register (RCC_CFGR) indicate which clock is currently used as a system clock.
Solved! Go to Solution.
2024-10-10 07:12 AM
Hello @MorganG ,
I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision.
Best regards,
Simon
2024-10-10 06:35 AM - edited 2024-10-10 07:21 AM
Hello @MorganG and welcome to the Community,
Thank you for raising this issue.
I will check this and will get back to you soon with update (Internal ticket is submitted ID 193408 - not available outside of ST)
2024-10-10 07:12 AM
Hello @MorganG ,
I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision.
Best regards,
Simon