2024-06-19 12:25 AM
Hello ST people,
I spotted an error in AN2834 rev 9, figure 8. Please refer to the image attached.
A negative offset error should be depicted in figure 8, but it is a positive offset error, just like in figure 7. To be a negative offset error, the actual transfer curve has to be offset to the left of the ideal transfer curve.
2024-06-19 01:18 AM - edited 2024-06-19 01:42 AM
Hello @ke1wa and welcome to the ST Community :smiling_face_with_smiling_eyes:
Thank you for reporting this. I've escalated to the Concerned team for more investigation and correction (under internal ticket number 184479). Thanks again for your contribution.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-19 08:32 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.