cancel
Showing results for 
Search instead for 
Did you mean: 

About STM32U858 Flash ECC error

pangpang
Visitor

According to the description of Section 7.3.2 "Error code correction (ECC)" in the RM0456 manual, reading the data at address 0x0BFA1F80 is supposed to generate an NMI interrupt.
However, when I tried to read the data at this address, no NMI interrupt was triggered.
I was also able to read the data at this address normally using Cube Programmer.
The development board used for testing is the ST`s B-U585I-IOT02A.
Why didn't the read operation trigger an NMI interrupt?

0 REPLIES 0