2021-12-13 5:51 AM
Hi
. I am using STM32L010C6tx processor. I drew the circuit myself. I did SYS-> debug serial wire. I was able to install without any problem. But sometimes "Memory Programming...
Opening and parsing file: ST-LINK_GDB_server_a14408.srec
File : ST-LINK_GDB_server_a14408.srec
Size: 19268 Bytes
Address: 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 150]
Error: failed to erase memory
Error: failed to erase memory
ST-LINK device status: UNKNOWN
CM3 Failed to print all registers
FAILED to REGISTER Values from the target
Debugger connection lost.
Shutting down...
" I'm getting it. I can't fix it. Any ideas?
Solved! Go to Solution.
2024-04-04 3:39 AM
Hi, ZKURT.1
I am also facing same problem
I tried with IDE 12.0, 15.0, 14.0
CUBEMX 6.10
I tried Full chip Erase through Cube Programmer but it's not working.
i cleaned the processor with a new one means what u did exactly?
Log output file: C:\Users\MQSTEC~1\AppData\Local\Temp\STM32CubeProgrammer_a13108.log
ST-LINK SN : 0673FF555551847167202052
ST-LINK FW : V2J44M29
Board : 32F769IDISCOVERY
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev A
Device name : STM32F76x/STM32F77x
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a13108.srec
File : ST-LINK_GDB_server_a13108.srec
Size : 10.25 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Error: failed to erase memory
Error: failed to erase memory
Shutting down...