2025-07-03 10:41 PM - last edited on 2025-07-04 12:27 AM by mƎALLEm
Hi,
I am working on NUCLEO-H743ZI EVK to test the secure boot using X-CUBE-SBSFU-v2.7.0 package.
I have successfully uploaded the boot image at the location 0x8000000 address and i have uploaded the userapp.sbf file using tera-term tool.
I have followed the user manual of Getting started with the X-CUBE-SBSFU STM32Cube Expansion Package - User manual for all my set up.
And now i just want to erase the flash memory using stm32cubeprogrammer tool but am unable to flash the normal led application after erasing.
Please look into the images mentioned below for your reference.
1. The below error is coming when uploading the basic led example.
Error: Failed to read memory at address 0x08000000 during verification
Error: Download verification failed
2. Settings of RDP and Boot Option Bytes
3. Settings of write protection
4. Settings of ST-LINK connection
4. The below image is my first uploaded userapp A.
Please guide me on how to erase the flash memory fully using programmer tool.
Thanks
Solved! Go to Solution.
2025-07-10 3:44 AM
Your flash is likely locked or write-protected. Set RDP to Level 0, disable write protection, do a full chip erase, then reset the board. After that, you should be able to upload your program.
2025-07-10 3:18 AM
Hello @kumar1 ,
it looks like you have changed the default settings in secure protections, but you left the write protection active. You need to remove it in option bytes.
Best regards
Jocelyn
2025-07-10 3:44 AM
Your flash is likely locked or write-protected. Set RDP to Level 0, disable write protection, do a full chip erase, then reset the board. After that, you should be able to upload your program.
2025-07-16 5:11 AM
Thanks for the reply.
I have successfully erased the chip using programmer tool by changing the PCROP address and disabled write protection.