cancel
Showing results for 
Search instead for 
Did you mean: 

Putting STM32L452 Sleep Mode

jkfc95
Associate

I'm developing a board with an STM32L452 and would like to find out if I can low the power consumption.
The current draining is 35mA, my goal is lower it to 20mA or less to achieve a requirement.
I've tried putting the device to sleep putting SLEEP MODE or STOP 1 MODE using the followings code:

while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

    HAL_Delay(1000);
    HAL_SuspendTick();
    HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON,PWR_SLEEPENTRY_WFI);
    HAL_ResumeTick();

}

or

while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

    HAL_Delay(1000);
    HAL_SuspendTick();
    HAL_PWREx_EnterSTOP0Mode(PWR_SLEEPENTRY_WFI);
    HAL_ResumeTick();
}
/* USER CODE END 3 */

But I can not see any change in my current. Still Draining 35mA.
Any help would be appreciate it.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Sarra.S
ST Employee

Hello @jkfc95, welcome to ST Community 

With these values, I believe you're not successfully entering Sleep/stop0 mode at all. 

As the expected Idd value in sleep mode is around 0.83mA and decreases when increasing Fhclk.

Could you please describe more the conditions (Fhclk clocking, peripherals enabled, RTC disabled/enabled, WKUP source, debug on?) 

Also, check this wiki article 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.