2021-05-17 09:29 AM
Hi,
I have a new project which should use only parts with life time of around 10 years. Where can I see on ST's website these information for a MCU?
Solved! Go to Solution.
2021-05-17 09:33 AM
You will find it at the product longevity website.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-05-17 09:33 AM
You will find it at the product longevity website.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-05-17 09:35 AM
See:
Most (all?) are 10 years starting Jan 2021. Based on history, these dates are likely to be extended even further.
2021-05-17 09:38 AM
Thanks a lot for your fast answer.
2021-05-17 09:45 AM
All STM32 are part of the so-called rolling commitment, which annually reviews the foreseeable market demand for each individual family (STM32F0, STM32F1, etc.) over the next 10 years. It cannot be seen that the demand for a family will decrease - on the contrary.
2021-05-22 04:43 AM
If the price of, for example, STM32F207VC would come down to the same as a STM32F107VC, then people would at least stop putting F1 into new designs and move to F2. 🙂