cancel
Showing results for 
Search instead for 
Did you mean: 

Duplicated code in stm32l0xx_hal_pcd.c V1.8.0

Daniel Atanasov
Associate
Posted on January 22, 2017 at 00:58

Hello,

I just started a mini project using USB CDC with STM32CubeMX and while trying to figure out how to use CDC driver i found this piece of code.

I think there is code duplication (copy-paste) in STM32Cube_FW_L0_V1.8.0/Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_pcd.c

In function PCD_EP_ISR_Handler(),

In section /* Decode and service non control endpoints interrupt  */ for Correct Transfer for transmission,

from /* IN double Buffering*/ to /*multi-packet on the NON control OUT endpoint*/.

Code in above described section wrongly writes data to PMA memory.

The later call to HAL_PCD_EP_Transmit() writes right data to PMA memory and sends it.

Possible side effect with duplicated code in PCD_EP_ISR_Handler() can be a calling of function PCD_FreeUserBuffer() twice in case of ep->doublebuffer != 0U.

#stm32l0xx
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Darius B
Associate II
Posted on March 16, 2018 at 15:21

Hello,

I found same necessaries memory copies   USB_WritePMA  in  PCD_EP_ISR_Handler 

at file stm32l4xx_hal_pcd.c

Project was generated with CubeX v4.24, STM32L4 package version 1.11.0

static HAL_StatusTypeDef PCD_EP_ISR_Handler(PCD_HandleTypeDef *hpcd)

{

......................

      if ((wEPVal & USB_EP_CTR_TX) != 0)

      {

        ep = &hpcd->IN_ep[epindex];

        

        /* clear int flag */

        PCD_CLEAR_TX_EP_CTR(hpcd->Instance, epindex);

        

        /* IN double Buffering*/

        if (ep->doublebuffer == 0)

        {

            /* necessaries memory copies  (copy paste problem from RX part?)

          ep->xfer_count = PCD_GET_EP_TX_CNT(hpcd->Instance, ep->num);

          if (ep->xfer_count != 0)

          {

            USB_WritePMA(hpcd->Instance, ep->xfer_buff, ep->pmaadress, ep->xfer_count);

          }*/

        }

        else

        {

           

//If double buffer not

incomprehensible code in red. Maybe stm software engineers or guru can explain it?

          if (PCD_GET_ENDPOINT(hpcd->Instance, ep->num) & USB_EP_DTOG_TX)

          {

            /*read from endpoint BUF0Addr buffer*/

            ep->xfer_count = PCD_GET_EP_DBUF0_CNT(hpcd->Instance, ep->num);

            if (ep->xfer_count != 0)

            {

              USB_WritePMA(hpcd->Instance, ep->xfer_buff, ep->pmaaddr0, ep->xfer_count);

            }

          }

          else

          {

            /*read from endpoint BUF1Addr buffer*/

            ep->xfer_count = PCD_GET_EP_DBUF1_CNT(hpcd->Instance, ep->num);

            if (ep->xfer_count != 0)

            {

              USB_WritePMA(hpcd->Instance, ep->xfer_buff, ep->pmaaddr1, ep->xfer_count);

            }

          }

          PCD_FreeUserBuffer(hpcd->Instance, ep->num, PCD_EP_DBUF_IN);  

        }

        /*multi-packet on the NON control IN endpoint*/

        ep->xfer_count = PCD_GET_EP_TX_CNT(hpcd->Instance, ep->num);

        ep->xfer_buff+=ep->xfer_count;

       

        /* Zero Length Packet? */

        if (ep->xfer_len == 0)

        {

          /* TX COMPLETE */

          HAL_PCD_DataInStageCallback(hpcd, ep->num);

        }

        else

        {

          HAL_PCD_EP_Transmit(hpcd, ep->num, ep->xfer_buff, ep->xfer_len);

        }

      }

............

}

BR.

Darius Babrauskas