2025-04-16 2:55 PM
Hi there,
I have the following setup duplicated thrice in my project - to select three distinct parameters to define an object.
Each listLayout is programmatically populated with a number of items (buttons).
One screen has 5 items, the other two have 6. Five items fit perfectly on a screen and don't require a scrollbar, while six items require scrolling to see the final item.
However, none of the scrollableContainer display their scrollbar until I touch the screen, despite me configuring it to do so (at least, that's what I think "Show scrollbars" means):
What am I doing wrong? How can I ensure that the vertical scroll bar is shown, by default, when I open a screen with more items than fit on a screen?
Thanks,
Julia
Solved! Go to Solution.
2025-04-18 10:07 AM
I couldn't figure out how to set this in TouchGFX Designer, but I was successfull at setting it programmatically, like so:
scrollableContainer.setScrollbarsPermanentlyVisible(true);as I'd learned in the TouchGFX docs.
I only have the vertical scrollbar set as visible, and it now appears as soon as I open the screen with this item.
2025-04-18 10:07 AM
I couldn't figure out how to set this in TouchGFX Designer, but I was successfull at setting it programmatically, like so:
scrollableContainer.setScrollbarsPermanentlyVisible(true);as I'd learned in the TouchGFX docs.
I only have the vertical scrollbar set as visible, and it now appears as soon as I open the screen with this item.
2025-04-18 10:30 AM
This combo works for me in 4.25